2025-05-21 3:20 AM
Hi
Is it posssible and if yes, is it plan to have Zephyr on the m33 core of the STM32MP257F-dk board ?
The NPU used in the STM32MP257FAK3 soc (used if I understand right on the STM32MP257F-dk board) is the same used in the Stm32 N6 board ?
Thanks
2026-02-12 1:36 PM
Yes, m33 core is supported on zephyr rtos, i'm curently making a project on it, see this guide