Usage of HAL_PCDEx_SetTxFiFo() when using DMA
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-07-23 10:34 PM
Hello,
I am trying to implement a Hi-Speed USB Device on STM32 baremetal project for STM32MP131Axx by using STM32Cube_FW_MP13_V1.1.0.
I am using the internal DMA of USB OTG to get faster the bulk transfer. I have 2 questions since I would like to know the suitable FIFO size when using the internal DMA.
Q1
I found the following comment in HAL_PCDEx_SetTxFiFo() function in stm32mp13xx_hal_pcd_ex.c.
When DMA is used 3n * FIFO locations should be reserved for internal DMA registers
I am using the endpoint 1 as bulkout that the max packet size is 512 bytes. In this case, is the comment mean that I need to pass 384 words to HAL_PCDEx_SetTxFiFo() as below?
HAL_PCDEx_SetTxFiFo(&hpcd,
1, // Use DIEPTXF1 for endpoint 1.
0x180); // 384 words = 1536 bytes
Q2
I refered the following post. Is it same for STM32MP13 line that I should not allocate more than (4096 – 72 (for DMA descs)) bytes in total -> 0x3EE words when using DMA?
Best regards,
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-09-29 6:50 PM
I also have a similar problem. Have you solved it?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-10-30 2:37 AM
Hello,
I am not certain, but I follow the rules below that are related my questions above. I use the internal DMA and I do not observe any issue for now.
- Allocates triple the size of the packet size to FIFO.
- Total allocated FIFO size should be less than 0x3ee words.
The following code shows FIFO allocation in my program. I hope this helps.
// Rx packet sizes
// control transfer in 64 bytes
// bulk transfer in 512 bytes
// total 576 bytes
//
// Sets triple the total packet size of 1728 bytes.
// Neess to pass the 4 bytes unit value, 1728 / 4 = 432 (0x1b0).
HAL_PCDEx_SetRxFiFo(&hpcd, 0x1b0);
// Tx packet size of endpoint 0
// control transfer out 64 bytes
//
// Sets triple the packet size of 192 bytes.
// Neess to pass the 4 bytes unit value, 192 / 4 = 48 (0x30).
HAL_PCDEx_SetTxFiFo(&hpcd, 0, 0x30);
// Tx packet size of endpoint 1
// bulk transfer out 512 bytes
//
// Sets triple the packet size of 1536 bytes.
// Neess to pass the 4 bytes unit value, 1536 / 4 = 384 (0x180).
HAL_PCDEx_SetTxFiFo(&hpcd, 1, 0x180);
// Total allocated fifo size is 0x1b0 + 0x30 + 0x180 = 0x360 words.
// It is less than 0x3ee words.
Best regards,