2026-02-05 7:27 PM - edited 2026-02-26 9:43 PM
Hi,
In STM32MP25x Reference manual(RM0457), the HSEM_(S)Cnxxx registers all have the description of global access attribute except HSEM_CnIER,
as shown of HSEM_CnICR,
22.5.4 HSEM non-secure interrupt clear register (HSEM_CnICR)
Address offset: 0x104 + 0x010 * (n - 1), (n = 1 to 3)
Reset value: 0x0000 0000
Register global access: When CID filtering for processor[n] is enabled in
HSEM_CnCIDCFGR, this register can be accessed only by the processor CID. An illegal
CID access to this register generates a CID illegal access event. When CID filtering for
processor[n] is disabled this register can be accessed by any bus master.
the HSEM_SCnIER also have the description of global access attribute, and the bits of HSEM_CnIER register also have CID filtering access attribute, and all bits maybe could be used by one CID , So if HSEM_CnIER also have the global access attribute?
2026-02-26 6:23 AM
Hello,
I'm not sure I understood the question to its full extent but I'll try to respond.
HSEM_CnIER register CID filtering is either:
Exemple, BIT(16) of HSEM_G1CIDCFGR is set => Proc1 CID defined in HSEM_C1CIDCFGR can access semaphores p = 0 Group HSEM3:0. If it was BIT(17), then it would be the CID of the proc2 defined in HSEM_C2CIDCFGR. It's a bitfield so I guess multiple proc can be white-listed.
I hope this helps,
Gatien
2026-02-26 10:00 PM
Hi,Gatien,
Yes, the attribute of the bit in HSEM_CnIER is clearly.
I mainly just want to confirm that , since the HSEM_SCnIER register and HSEM_CnICR register all have the attribute of "Register global access", does the HSEM_CnIER register also have this attribute?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.