cancel
Showing results for 
Search instead for 
Did you mean: 

Enable analyzers on the CubeIDE

SteMMo
Senior

Hi there,

I'm working on a STM32MP135 project.

I'd like to see some information on the Build Analyzer and/or Static stack analyzer but they always report the grids empty.

The project is compiled with the -fstack-usage and debualt Debug level (-g).

I checked that for each source files of the project are generated the .cyclo, .su, .d and .o files in the Debug directory.

The analyzers windows do not have a button to associate the project: but it seems not to be a problem with the latest relases.

So, why I cannot browse the analyzers data?

 

Version: 1.19.0

Build: 25607_20250703_0907 (UTC)

 

Thanks, regards

1 ACCEPTED SOLUTION

Accepted Solutions
Souhaib MAZHOUD
ST Employee

Hello @SteMMo 

It seems that this is the same issue being discussed here.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
SteMMo
Senior

I've found that 'sometimes' works the 'Refresh' button .. sometimes .. the binaries are always rebuilt.

 

Souhaib MAZHOUD
ST Employee

Hello @SteMMo 

It seems that this is the same issue being discussed here.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.