2023-01-12 2:39 PM
Hi,
I try to couple LCD TFT ili9881c (mipi dsi 2 lanes interface) with stm32mp157caa3.
My custom driver seems to be loading correctly.
When I type lsmod I get
Module Size Used by
cfg80211 651264 0
usb_f_rndis 24576 2
u_ether 20480 1 usb_f_rndis
libcomposite 49152 10 usb_f_rndis
galcore 516096 2
panel_ilitek_ili9881c 20480 0
dwmac_stm32 16384 0
stmmac_platform 20480 1 dwmac_stm32
stm32_adc_core 20480 0
spi_stm32 24576 0
sch_fq_codel 20480 3
ip_tables 24576 0
x_tables 24576 1 ip_tables
ipv6 512000 42Unfortunately, the display is not working, only the backlight is working.
I checked twice the dts and looks good, driver is loading well. I can't find anything with 'drm'. What I missed? Shall I add some additional driver in the kernel or something install in the roofs?
In the log, I can see only
[ 0.079013] platform 5a000000.dsi: Fixing up cyclic dependency with 5a001000.display-controllerand
[ 13.730531] [drm] Initialized stm 1.0.0 20170330 for 5a001000.display-controller on minor 0
Solved! Go to Solution.
2023-03-30 3:07 AM
I think I can close this topic. The real problem is related with display itself. STM32MP1x support only 2 lane displays. My display have 4 lane and it can't be reconfigured by software to 2 lane - missing access to IM pins. So I think mipi works but the display can't be handled by 2 lanes.
2023-01-13 8:28 AM
Hello @Michał Wołowik ,
Can you tell me on which linux version you are working on ? 5.10 or 5.15 (DV 3.1 or 4.1 ?)
You mentioned your "custom driver" for ili9881 panel. Does it mean that you did not take the one upstreamed under <linux_folder>/drivers//gpu/drm/panel/panel-ilitek-ili9881c.c ?
Can you also share your device tree ?
Kind regards,
Erwan.
2023-01-13 9:02 AM
2023-01-13 10:43 AM
I also check other not modified drivers, the result is the same.
Nothing on the MIPI lines and in the log.
/* compatible = "winstar,WF50DTYA3MNG10", "ilitek,ili9881c"; */
compatible = "raydium,rm68200";I think I missed something due I start designing dts from Cube Mx.
2023-01-16 12:15 AM
Hello @Michał Wołowik,
Looking at your shared files, I do not see obvious issue that can explain your problem.
Are you working on a custom board or is it the stm32mp157c-dk2 board ?
Just to get a little bit more information, we can take a look at the following things:
Kind regards,
Erwan.
2023-01-16 1:04 AM
2023-01-18 7:14 AM
Hello @Michał Wołowik ,
Are you able to probe the different signals in entry of your panel ?
Do you see the pixel clock etc or nothing ?
Can you provide a full boot log file with "dmsg" command ?
Kind regards,
Erwan.
2023-01-18 7:27 AM
@Michał Wołowik ,
Sorry for the DRM logs I was not really clear. In fact I would like to see the DRM logs at boot time.
You can enable it with adding "drm.debug=0x2" in the Linux commandline (0x2 will display drivers message only).
In ST deliveries, we can modify it on bootfs partition in extlinux.conf files.
For example, with my stm32mp157f-dk2 I will have:
root@stm32mp1:/boot/mmc0_extlinux# cat stm32mp157f-dk2_extlinux.conf
# Generic Distro Configuration file generated by OpenEmbedded
menu title Select the boot mode
MENU BACKGROUND /splash.bmp
TIMEOUT 20
DEFAULT OpenSTLinux
LABEL OpenSTLinux
KERNEL /uImage
FDTDIR /
INITRD /uInitrd
APPEND root=PARTUUID=e91c4e10-16e6-4c0e-bd0e-77becf4a3582 rootwait rw console=ttySTM0,115200 drm.debug=0x2
LABEL stm32mp157f-dk2-a7-examples
KERNEL /uImage
FDT /stm32mp157f-dk2-a7-examples.dtb
INITRD /uInitrd
APPEND root=PARTUUID=e91c4e10-16e6-4c0e-bd0e-77becf4a3582 rootwait rw console=ttySTM0,115200
LABEL stm32mp157f-dk2-m4-examples
KERNEL /uImage
FDT /stm32mp157f-dk2-m4-examples.dtb
INITRD /uInitrd
APPEND root=PARTUUID=e91c4e10-16e6-4c0e-bd0e-77becf4a3582 rootwait rw console=ttySTM0,115200and at boot time, the following DRM traces are displayed:
[ 0.000000] Kernel command line: root=PARTUUID=e91c4e10-16e6-4c0e-bd0e-77becf4a3582 rootwait rw console=ttySTM0,115200 drm.debug=0x2
[ 3.118656] [drm:ltdc_load]
[ 3.662669] [drm:ltdc_load]
[ 4.219836] [drm:ltdc_load]
[ 4.219954] [drm:ltdc_load] Bridge encoder:31 created
[ 4.220011] [drm:ltdc_load] Bridge encoder:33 created
[ 4.220201] [drm:ltdc_load] ltdc hw version 0x00010300
[ 4.220839] [drm:ltdc_plane_create] plane:35 created
[ 4.220869] [drm:ltdc_load] CRTC:37 created
[ 4.220890] [drm:ltdc_plane_create] plane:38 created
[ 4.220898] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 4.226124] [drm] Driver supports precise vblank timestamp query.
[ 4.233250] [drm] Initialized stm 1.0.0 20170330 for 5a001000.display-controller on minor 0
[ 9.915889] [drm:ltdc_crtc_mode_valid] clk rate target 29700000, available 29700000
[ 9.945755] [drm:ltdc_crtc_mode_valid] clk rate target 29700000, available 29700000
[ 9.945787] [drm:ltdc_crtc_mode_fixup] requested clock 29700kHz, adjusted clock 29700kHz
[ 9.945799] [drm:ltdc_plane_atomic_check]
[ 9.945815] [drm:ltdc_plane_atomic_check] plane:35 fb:40 (480x800)@(0,0) -> (480x800)@(0,0)
[ 9.945873] [drm:drv_runtime_resume]
[ 9.945882] [drm:ltdc_resume]
[ 9.945912] [drm:ltdc_crtc_mode_set_nofb] CRTC:37 mode:480x800
[ 9.945923] [drm:ltdc_crtc_mode_set_nofb] Video mode: 480x800
[ 9.945954] [drm:ltdc_crtc_mode_set_nofb] hfp 98 hbp 98 hsl 32 vfp 15 vbp 14 vsl 10
[ 9.945975] [drm:ltdc_encoder_mode_set]
[ 9.946107] [drm:dw_mipi_dsi_get_lane_mbps] pll_in 24000kHz pll_out 428000kHz lane_mbps 428MHz
[ 9.958729] [drm:dw_mipi_dsi_mode_set] failed to wait phy lock state
[ 10.015631] [drm:ltdc_plane_atomic_update] fb: phys 0xd2200000
[ 10.015650] [drm:ltdc_crtc_enable_vblank]
[ 10.015686] [drm:ltdc_crtc_atomic_enable]
[ 10.814514] [drm:ltdc_encoder_enable]
[ 10.814534] [drm:dw_mipi_dsi_phy_power_on]
[ 15.845557] [drm:ltdc_crtc_disable_vblank] Kind regards,
Erwan.
2023-01-18 9:25 AM
Hi Erwan,
drm boot log
root@stm32mp1-computer-lcd:~# dmesg | grep drm
[ 0.000000] Kernel command line: root=PARTUUID=491f6117-415d-4f53-88c9-6e0de54deac6 rootwait rw drm.debug="0x02" console=ttySTM0,115200
[ 0.500555] [drm:ltdc_load]
[ 2.249006] [drm:ltdc_load]
[ 2.249178] [drm:ltdc_load] Bridge encoder:31 created
[ 2.249483] [drm:ltdc_load] ltdc hw version 0x00010300
[ 2.267527] [drm:ltdc_plane_create] plane:33 created
[ 2.267605] [drm:ltdc_crtc_init] CRTC:37 created
[ 2.267645] [drm:ltdc_plane_create] plane:38 created
[ 2.278255] [drm] Initialized stm 1.0.0 20170330 for 5a001000.display-controller on minor 0
[ 9.426142] systemd[1]: Starting Load Kernel Module drm...
[ 10.745919] [drm:ltdc_crtc_mode_valid] clk rate target 54000000, available 54000000
[ 10.792624] [drm:ltdc_crtc_mode_valid] clk rate target 54000000, available 54000000
[ 10.792725] [drm:ltdc_crtc_mode_fixup] requested clock 54000kHz, adjusted clock 54000kHz
[ 10.792754] [drm:ltdc_plane_atomic_check]
[ 10.792827] [drm:drv_runtime_resume]
[ 10.792863] [drm:ltdc_resume]
[ 10.792914] [drm:ltdc_crtc_mode_set_nofb] CRTC:37 mode:720x1280
[ 10.792938] [drm:ltdc_crtc_mode_set_nofb] Video mode: 720x1280
[ 10.792960] [drm:ltdc_crtc_mode_set_nofb] hfp 48 hbp 48 hsl 9 vfp 12 vbp 12 vsl 5
[ 10.793045] [drm:ltdc_encoder_mode_set]
[ 10.793146] [drm:dw_mipi_dsi_get_lane_mbps] pll_in 24000kHz pll_out 776000kHz lane_mbps 776MHz
[ 10.807297] [drm:dw_mipi_dsi_mode_set] failed to wait phy lock state
[ 10.867439] [drm:dw_mipi_dsi_phy_power_on]
[ 10.867508] [drm:ltdc_plane_atomic_update] plane:33 fb:42 (720x1280)@(0,0) -> (720x1280)@(0,0)
[ 10.867575] [drm:ltdc_plane_atomic_update] fb: phys 0xc3900000
[ 10.867615] [drm:ltdc_crtc_atomic_enable]
[ 11.257293] [drm:ltdc_encoder_enable]
[ 11.257376] [drm:ltdc_crtc_enable_vblank]
[ 16.317225] [drm:ltdc_crtc_disable_vblank]
[ 18.130419] [drm:ltdc_plane_atomic_check]
[ 18.130532] [drm:drm_atomic_helper_commit_planes] CRTC:37 plane:33
[ 18.130579] [drm:ltdc_crtc_enable_vblank]
[ 23.197261] [drm:ltdc_crtc_disable_vblank]
[ 27.588309] [drm:ltdc_crtc_mode_valid] clk rate target 54000000, available 54000000
[ 27.695429] [drm:ltdc_plane_atomic_check]
[ 27.695491] [drm:ltdc_plane_atomic_check]
[ 27.749367] [drm:ltdc_plane_atomic_check]
[ 27.749426] [drm:ltdc_plane_atomic_check]
[ 27.749556] [drm:ltdc_plane_atomic_update] plane:33 fb:42 (720x1280)@(0,0) -> (720x1280)@(0,0)
[ 27.749634] [drm:ltdc_plane_atomic_update] fb: phys 0xce400000
[ 27.749669] [drm:ltdc_crtc_enable_vblank]
[ 29.098611] [drm:ltdc_plane_atomic_check]
[ 29.343705] [drm:ltdc_plane_atomic_check]
[ 29.343911] [drm:ltdc_plane_atomic_update] plane:33 fb:43 (720x1280)@(0,0) -> (720x1280)@(0,0)full log in the attachment.
BR Michal
2023-01-18 9:30 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.