cancel
Showing results for 
Search instead for 
Did you mean: 

M4 GPIO realistic maximal frequency ?

DBuer
Associate II

How long does it take (approx) to rise or lower a GPIO pin fix configured to the M4 in the STM32MP157c, after issuing the command in the M4 code ? On our native STM32F409 board it takes around 10ns. I'm afraid the STM32MP1xx is much slower right ?

Regards,

Daniel

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Olivier GALLIEN
ST Employee

Hi @DB.7uergin​ 

Once a GPIO is allocated to M4 context there is no difference driving a GPIO from an MP1 M4 or STM32F4.

So no reason for a specific overhead here.

Did you measure something different to make this assumption ?

Br,

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hi Oliver

Ok thanks that sounds good. No i didn't measure anything on the MP1 Board, but i've made some bad experiences with other boards (i.MX7dual) where the GPIOs are quite slow (150 - 200ns) to raise or lower.

So it should be enough to lock my GPIO with "PERIPH_LOCK()" inside the M4 at the beginning of my code or do i need to update the DeviceTree ? I'm not sure if i already understood the ways of allocating the resources to either side (A7 or M4) :)

But anyway thanks for the answer.

Daniel

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.