cancel
Showing results for 
Search instead for 
Did you mean: 

How to work with A7-core with IAR?

Hungchul.Shin
Associate II

Can't a7-core write firmware with a generic compiler like IAR without Linux?

Like working with tools like ADS Compiler , like s3c6440 .....

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2

You can compile with GNU/GCC running under Windows.​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Ozone
Principal III

You need to check if the compiler supports the specific core (Cortex A7), and the toolchain comes with the required environment (Linux header files, device-specific drivers, and libs).

Microcontroller specific ones like IAR and Keil usually do not.