2019-09-18 3:38 AM
The hardware is STM32MP157C-DK2 board.
1. We setup the test environment as below:
We bridge the USB port and the Ethernet port in the ST.
The throughput is about 270Mbit/sec(Limited by the usb to Ethernet convertor).
2. Another test environment is:
The ST is using the USB gadget functions. The USB port and the Ethernet port are bridged.
Result:
RNDIS: 90Mbit/sec.
CDC-EEM: 110Mbit/sec.
CDC-ECM: 135Mbit/sec.
The performance is not good enough compared to test1.
Is the speed limited by the USB-OTG controller(dwc2)?
Can we change the DMA settings in the dwc2 ?
Or anyway to improve the throughput?
Please help!
Thank you very much.
2019-10-10 8:27 AM
Hi,
The way to improve the throughput is to tune FIFO size in the OTG IP. It can be done through kernel device tree.
In usbotg_hs entry of arch/arm/boot/dts/stm32mp157c.dtsi :
usbotg_hs: usb-otg@49000000 {
compatible = "st,stm32mp1-hsotg", "snps,dwc2";
reg = <0x49000000 0x10000>;
clocks = <&rcc USBO_K>;
clock-names = "otg";
resets = <&rcc USBO_R>;
reset-names = "dwc2";
interrupts-extended = <&intc GIC_SPI 98 IRQ_TYPE_LEVEL_HIGH>,
<&exti 44 1>;
interrupt-names = "event", "wakeup";
g-rx-fifo-size = <256>;
g-np-tx-fifo-size = <32>;
g-tx-fifo-size = <128 128 64 64 64 64 32 32>;
dr_mode = "otg";
usb33d-supply = <&usb33>;
power-domains = <&pd_core>;
wakeup-source;
status = "disabled";
};The following patch increases tx troughput (I measured a gain of 12% in TX):
- g-np-tx-fifo-size = <32>;
- g-tx-fifo-size = <128 128 64 64 64 64 32 32>;
+ g-np-tx-fifo-size = <256>;
+ g-tx-fifo-size = <128 128 64 16 16 16 16 16>The sum of all FIFO size must be lower than 952.
Depending on your use case, you can tune FIFO sizes to get the best compromise.
BR,
Christophe