2025-03-06 2:31 AM
I have created a button in qt when I click on the button it has to create a pdf and also display the pdf.
i am developing an application where i have to store the user data in pdf called report and later view it
please give me the steps on how to perform this and any examples related to it
2025-03-10 6:43 AM
Hello @Sharan ,
STMicroelectronics brings the necessary support to develop and use your Qt application to make it run on the target, but this question sounds more like a Qt specific topic.
I think the Qt official documentation or Qt forum could help you more than we can.
Kind regards,
Erwan.
2025-03-23 11:58 PM - edited 2025-03-24 12:12 AM
how to open a pdf file from my terminal in stm32mp157d-dk1
root@stm32mp15-disco:~# xdg open mydoc.pdf
-sh: xdg: not found
root@stm32mp15-disco:~# okular mydoc.pdf
-sh: okular: not found
root@stm32mp15-disco:~# evince mydoc.pdf
-sh: evince: not found
root@stm32mp15-disco:~# mupdf mydoc.pdf
-sh: mupdf: not found
root@stm32mp15-disco:~#
2025-03-31 5:41 AM
Seems there is an example how to read/show pdf in Qt:
https://doc.qt.io/qt-6/qtpdf-pdfviewer-example.html
For creating PDFs, there are tons of libraries, some of them open-source.
2025-04-14 11:38 PM
I am using QT 5.15.13 for my stm32mp157d-dk1 and the image does not have any pdf opener and i have upgraded my qt to 6.7.3 can i use this version for developing application because when i use ssh and connect to the stm32mp and when i type qmake it shows
using qt version 5.15.13 in /usr/lib