2023-03-16 5:15 PM
Hi,
I try to connect ADC channels with libiio for my custom board based on the stm32mp157caa3. I followed the instructions from the link
https://wiki.st.com/stm32mpu/wiki/IIO_libiio
https://wiki.st.com/stm32mpu/wiki/ADC_device_tree_configuration#DT_configuration_examples
but without success. After issuing the console
iio_infoI get
Library version: 0.23 (git tag: 92d6a35)
Compiled with backends: local xml ip usb serial
IIO context created with local backend.
Backend version: 0.23 (git tag: 92d6a35)
Backend description string: Linux stm32mp1-connect-bridge 5.15.67 #1 SMP PREEMPT Thu Sep 8 10:32:54 UTC 2022 armv7l
IIO context has 2 attributes:
local,kernel: 5.15.67
uri: local:
IIO context has 0 devices:The same is in
/sys/bus/iio/devices/empty, with no devices.
Part of my dts looks
&adc{
pinctrl-names = "default", "sleep";
pinctrl-0 = <&adc_pins_mx>;
pinctrl-1 = <&adc_sleep_pins_mx>;
status = "okay";
/* USER CODE BEGIN adc */
vdda-supply = <&vdda>; /* Example to supply vdda pin by using a PMIC regulator */
vref-supply = <&vrefbuf>; /* Example to use VREFBUF (It needs to be enabled as well) */
adc1: adc@0 {
assigned-resolution-bits = <12>;
/* Single-ended channels */
channel@0 {
reg = <0>;
st,min-sample-time-ns = <10000>; /* 10µs sampling time */
};
channel@1 {
reg = <1>;
st,min-sample-time-ns = <10000>; /* 10µs sampling time */
};
channel@2 {
reg = <2>;
st,min-sample-time-ns = <10000>; /* 10µs sampling time */
};
channel@3 {
reg = <3>;
st,min-sample-time-ns = <10000>; /* 10µs sampling time */
};
channel@5 {
reg = <5>;
st,min-sample-time-ns = <10000>; /* 10µs sampling time */
};
channel@6 {
reg = <6>;
st,min-sample-time-ns = <10000>; /* 10µs sampling time */
};
channel@9 {
reg = <9>;
st,min-sample-time-ns = <10000>; /* 10µs sampling time */
};
channel@10 {
reg = <10>;
st,min-sample-time-ns = <10000>; /* 10µs sampling time */
};
channel@12 {
reg = <12>;
st,min-sample-time-ns = <10000>; /* 10µs sampling time */
};
channel@13 {
reg = <13>;
st,min-sample-time-ns = <10000>; /* 10µs sampling time */
};
channel@15 {
reg = <15>;
st,min-sample-time-ns = <10000>; /* 10µs sampling time */
};
channel@17 {
reg = <17>;
st,min-sample-time-ns = <10000>; /* 10µs sampling time */
};
};
/* USER CODE END adc */
};In the Kernel configuration, I also marked
Device Drivers --->
<*> Industrial I/O support --->
Analog to digital converters --->
<*> STMicroelectronics STM32 adc core
<*> STMicroelectronics STM32 adcIt must be something I missed.
Thanks in advance for the hints.
BR Michal
Solved! Go to Solution.
2023-03-17 10:33 AM
Unfortunately, the result is the same. But I have an additional question. After writing my new image to sd card or in my case emmc what I should do after the first login? Maybe here is the problem, maybe additional configuration is needed?
2023-03-17 10:34 AM
When I issue lsmod I get
Module Size Used by
cfg80211 626688 0
usb_f_rndis 24576 2
u_ether 20480 1 usb_f_rndis
libcomposite 49152 10 usb_f_rndis
galcore 520192 0
dwmac_stm32 16384 0
stmmac_platform 20480 1 dwmac_stm32
stm32_adc_core 20480 0
spi_stm32 24576 0
stm32_timers 16384 0
sch_fq_codel 20480 3
ip_tables 24576 0
x_tables 24576 1 ip_tables
ipv6 503808 42on dk board, I see something different
stm32_adc 32768 0
stm32_timer_trigger 20480 1 stm32_adc
stm32_lptimer_trigger 16384 1 stm32_adcThe above means that timers use adc.
Where I should bind the timer with adc and how?
2023-03-17 11:48 AM
I have tried to unload the stm32_adc module and the adc devices were removed to. So try to execute modprobe stm32_adc. If this helps add a stm32-adc.conf to the /etc/modules-load.d/. This could help.
2023-03-17 12:08 PM
Now I'm able to achieve this
stm32_adc 32768 0
stm32_timer_trigger 20480 1 stm32_adc
stm32_lptimer_trigger 16384 1 stm32_adcbut after going to "/sys/bus/iio/devices" still empty
2023-03-17 12:10 PM
on disco I have
root@stm32mp13-disco:/sys/bus/iio/devices# ls
iio:device0 on my board
nothing
2023-03-17 12:14 PM
I just see that I have a snapshot distro
ST OpenSTLinux - Weston - (A Yocto Project Based Distro) 4.0.4-snapshotI try to repo sync and check.
2023-03-18 7:24 AM
Can you post dmesg, full device tree and check if there is anything interesting in /proc/device-tree/soc/adc@48003000/?
2023-03-18 9:44 AM
Hi,
.../sys/firmware/devicetree/base/soc/adc@48003000/adc@0# ls
I have
'#address-cells' compatible interrupt-parent reg
'#io-channel-cells' dma-names interrupts status
'#size-cells' dmas name
2023-05-08 10:09 AM
After some break and rechecking everything I discover a correct dts configuration.
First I used as reference AVDD(external) and according to this I have configurations like
The Kernel
&adc {
/* ANA0, ANA1 are dedicated pins and don't need pinctrl: only in6. */
pinctrl-names = "default", "sleep";
pinctrl-0 = <&adc_pins_mx>;
pinctrl-1 = <&adc_sleep_pins_mx>;
vdd-supply = <&vdd>;
vdda-supply = <&vdda>;
vref-supply = <&vdda>;
status = "okay";
adc1: adc@0 {
#address-cells = <1>;
#size-cells = <0>;
status = "okay";
channel@0 {
reg = <0>;
/* 16.5 ck_cycles sampling time */
st,min-sample-time-ns = <5000>;
};
channel@1 {
reg = <1>;
st,min-sample-time-ns = <5000>;
};
channel@3 {
reg = <3>;
st,min-sample-time-ns = <5000>;
};
channel@5 {
reg = <5>;
st,min-sample-time-ns = <5000>;
};
channel@6 {
reg = <6>;
st,min-sample-time-ns = <5000>;
};
channel@9 {
reg = <9>;
st,min-sample-time-ns = <5000>;
};
channel@10 {
reg = <10>;
st,min-sample-time-ns = <5000>;
};
channel@13 {
reg = <13>;
st,min-sample-time-ns = <5000>;
};
channel@15 {
reg = <15>;
st,min-sample-time-ns = <5000>;
};
};
};The U-Boot
&adc {
/* ANA0, ANA1 are dedicated pins and don't need pinctrl: only in6. */
pinctrl-names = "default", "sleep";
pinctrl-0 = <&adc_pins_mx>;
pinctrl-1 = <&adc_sleep_pins_mx>;
vdd-supply = <&vdd>;
vdda-supply = <&vdda>;
vref-supply = <&vdda>;
status = "okay";
adc1: adc@0 {
#address-cells = <1>;
#size-cells = <0>;
status = "okay";
channel@0 {
reg = <0>;
/* 16.5 ck_cycles sampling time */
st,min-sample-time-ns = <5000>;
};
channel@1 {
reg = <1>;
st,min-sample-time-ns = <5000>;
};
channel@3 {
reg = <3>;
st,min-sample-time-ns = <5000>;
};
channel@5 {
reg = <5>;
st,min-sample-time-ns = <5000>;
};
channel@6 {
reg = <6>;
st,min-sample-time-ns = <5000>;
};
channel@9 {
reg = <9>;
st,min-sample-time-ns = <5000>;
};
channel@10 {
reg = <10>;
st,min-sample-time-ns = <5000>;
};
channel@13 {
reg = <13>;
st,min-sample-time-ns = <5000>;
};
channel@15 {
reg = <15>;
st,min-sample-time-ns = <5000>;
};
};
};Finally T-Fa
&etzpc{
status = "okay";
st,decprot = <
/*"Non Secured" peripherals*/
DECPROT(STM32MP1_ETZPC_ADC_ID, DECPROT_NS_RW, DECPROT_UNLOCK)
...
}
and
&rcc{
...
CLK_ADC_PLL4R
pll4:st,pll@3 {
compatible = "st,stm32mp1-pll";
reg = <3>;
cfg = < 3 98 5 6 5 PQR(1,1,1) >;
};This works for me and maybe will be suitable for someone else.
Thanks for any help
Topic can be closed.