cancel
Showing results for 
Search instead for 
Did you mean: 

Where does tf-a-stm32mp157d-ev1-usb.stm32 come from ?

JSchn.5
Associate III

Our hardware has an STM32MP151DAx.

In order to make use of the Cube Programmer and the boot-via-USB method I need the equivalent of the tf-a-stm32mp157d-ev1-usb.stm32 file but for our hardware.

I have worked through the IOC stuff, have DTS files and got the hang of building TF-A (and U-Boot and Linux) according to instructions but how do I build this -USB variant as used in the .TSV files ?

Jon

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
PatrickF
ST Employee

Hi @JSchn.5​ ,

I'm not expert, but did you follow https://wiki.st.com/stm32mpu/wiki/How_to_compile_the_device_tree_with_the_Developer_Package#TF-A_-_regenerate_TF-A ?

The "xxxx-usb.stm32" bianry is generated during make with TF_A_CONFIG="optee emmc nand nor sdcard uart usb" option (could be tailored to your needs if you only need some flash flavors)

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here