STM32MP157C custom machine dts compile error
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-09-28 9:08 AM
So I got the basic yocto build working for the STM32MP157C-DK2 and have been able to modify it to add/ remove/ modify features without any problems both st-image-core and st-image-weston.
Then I come to do a custom machine and add it to the build by following:
https://wiki.st.com/stm32mpu/index.php/How_to_create_your_own_machine
This build runs until I get the following error:
arch/arm/dts/.stm32mp1-test.dtb.pre.tmp:14:10: fatal error: stm32mp157.dtsi: No such file or directory
| #include "stm32mp157.dtsi"
| ^~~~~~~~~~~~~~~~~
| compilation terminated.
I have a feeling I have missed something simple but any advice greatly appreciated.
- Labels:
-
STM32MP15 Lines
-
Yocto
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-09-29 5:09 AM
Hi @EButl.1​ ,
Could you please confirm you are using a complete and consistant ecosystem V2.0 delivery ?
Complete trace of Yocto build may help to analyze the issue.
Olivier
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-09-30 12:48 AM
So this is the script that I run for setting up the build
repo init -u https://github.com/STMicroelectronics/oe-manifest.git -b refs/tags/openstlinux-4.19-thud-mp1-19-10-09
repo sync
cd layers/meta-openembedded ; git checkout thud
cd ../meta-qt5 ; git checkout thud
cd ../meta-st/meta-st-openstlinux ; git checkout thud
cd ../meta-st-stm32mp ; git checkout thud
cd ../meta-st-stm32mp-addons ; git checkout thud
cd ../../meta-timesys ; git checkout thud
cd ../openembedded-core ; git checkout thud
cd bitbake ; git checkout 1.40
cd ../..
cp -r ../../../../meta-my-test-layer .
cd ../
mkdir git-repos
cd git-repos
git clone https://github.com/STMicroelectronics/STM32CubeMP1.git STM32CubeMP1.git
git clone https://github.com/STMicroelectronics/linux.git linux.git
cd ..
DISTRO=openstlinux-weston MACHINE=stm32mp1-test source layers/meta-st/scripts/envsetup.sh
bitbake st-image-weston
################################################################################################
The stm32mp1-test.conf is below:
#@TYPE: Machine
#@NAME: stm32mp1-test
#@DESCRIPTION: Configuration for STM32CubeMX generated project
#@NEEDED_BSPLAYERS: layers/meta-openembedded/meta-oe layers/meta-openembedded/meta-python
include conf/machine/include/st-machine-common-stm32mp.inc
include conf/machine/include/stm32mp1-mx-config.inc
include conf/machine/include/stm32mp1-mx-extlinux-config.inc
include conf/machine/include/stm32mp1-mx-common.inc
#require conf/machine/include/st-machine-common-stm32mp.inc
#require conf/machine/include/stm32mp1-mx-common.inc
# =========================================================================
# CubeMX extra config
# =========================================================================
# Set specific path by components for DT file location
CUBEMX_DTB_PATH_TFA = "${STM32MP_MX_BASE}/mx/${CUBEMX_PROJECT}/tf-a"
CUBEMX_DTB_PATH_UBOOT = "${STM32MP_MX_BASE}/mx/${CUBEMX_PROJECT}/u-boot"
CUBEMX_DTB_PATH_LINUX = "${STM32MP_MX_BASE}/mx/${CUBEMX_PROJECT}/kernel"
#CUBEMX_DTB_PATH_OPTEEOS = "${STM32MP_MX_BASE}/mx/${CUBEMX_PROJECT}/optee-os"
# =========================================================================
# User customizing sections
# =========================================================================
# Override machine specific OPTEE config with generic DK2 one
#OPTEE_CONF = "stm32mp157c-dk2"
# Boot Scheme
# =========================================================================
# DISCO / EVAL : basic, trusted or optee
# =========================================================================
#BOOTSCHEME_LABELS += "basic"
#BOOTSCHEME_LABELS += "trusted"
BOOTSCHEME_LABELS += "optee"
# Boot Device Choice
# =========================================================================
# DISCO : sdcard
# EVAL : sdcard, emmc, nand-4-256, nor-sdcard, nor-emmc or nor-nand-4-256
# =========================================================================
# Define the boot device supported
BOOTDEVICE_LABELS += "sdcard"
# WARNING: configs below are only available with EVAL board
#BOOTDEVICE_LABELS += "emmc"
#BOOTDEVICE_LABELS += "nand-4-256"
#BOOTDEVICE_LABELS += "nor-emmc"
#BOOTDEVICE_LABELS += "nor-nand-4-256"
# Board Type Choice
# =========================================================================
# DISCO : stm32mp157a-dk1 or stm32mp157c-dk2
# EVAL : stm32mp157c-ev1
# =========================================================================
# Define the board reference devicetree name
# WARNING: only one setting allowed
#CUBEMX_BOARD_REFERENCE = "stm32mp157a-dk1"
CUBEMX_BOARD_REFERENCE = "stm32mp157c-dk2"
#CUBEMX_BOARD_REFERENCE = "stm32mp157c-ev1"
# CubeMX Project Config
# =========================================================================
# Assign CubeMX Board devicetree and project path name
CUBEMX_DTB = "stm32mp1-test"
CUBEMX_PROJECT = "../../../../../../../stm32mp1-test/CA7/DeviceTree/stm32mp1-test"
###################################################################################################
All of the missing files are in the https://github.com/STMicroelectronics/linux.git repo but I'm not sure where I should make that reference/ include or should they be downloaded automatically?
I also tried copying the missing file but it has it's own dependencies that are required
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-09-30 12:52 AM
Also the installed ecosystem is STM32MP15-Ecosystem-v1.2.0
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-09-30 12:54 AM
Hi @EButl.1​
A possible issue is that you are using STM32CubeMX V6.0.x to generate your Device Tree which are only compliant with Ecosystem V2.0.
>> repo init -u https://github.com/STMicroelectronics/oe-manifest.git -b refs/tags/openstlinux-4.19-thud-mp1-19-10-09
This is the quite old V1.1 ecosystem Distribution !?
For compatibility you may need to use STM32CubeMX V5.4 !
Please check-out :
https://wiki.st.com/stm32mpu-ecosystem-v1/wiki/STM32MP15_ecosystem_release_note_-_v1.1.0#STM32CubeMX
Olivier
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-09-30 12:58 AM
Strange, Ecosystem V1.2 would have mean :
Openstlinux-20-02-19 not openstlinux-4.19-thud-mp1-19-10-09 you mention in above comment.
Olivier
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-10-13 12:51 AM
Hi,
You were right about the revisions. It turned out that the dts' were produced with ecosystem 2.0 and were incompatible with the 4.9.
I moved over to the 5.4 Dunfell branch and was able to generate the dtbs.
I did notice that even when building a default image that build does not work straight out of the box, I'll get a few notes up here once I have have done a couple of clean builds and am happy it is working.
Thanks again.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-10-14 3:09 AM
So as promised a brief description on building the basic image with 5.4
(taken from a bash file I use to build it)
mkdir bin
PATH=$PWD/bin:$PATH
curl https://storage.googleapis.com/git-repo-downloads/repo > bin/repo
chmod a+x bin/repo
mkdir testBuild
cd testBuild
mkdir yocto
cd yocto
repo init -u https://github.com/STMicroelectronics/oe-manifest.git -b refs/tags/openstlinux-5.4-dunfell-mp1-20-06-24
repo sync
cd layers/meta-openembedded ; git checkout dunfell
cd ../meta-qt5 ; git checkout dunfell
cd ../meta-st/meta-st-openstlinux ; git checkout dunfell
cd ../meta-st-stm32mp ; git checkout dunfell
cd ../meta-st-stm32mp-addons ; git checkout dunfell
cd ../../meta-timesys ; git checkout dunfell
cd ../openembedded-core ; git checkout dunfell
cd bitbake ; git checkout 1.46
cd ../..
cp -r ../../../../meta-my-test-layer .
cd ../
# These were breaking the build
rm layers/meta-st/meta-st-openstlinux/recipes-multimedia/v4l2apps/v4l-utils_1.18.0.bbappend
rm layers/meta-st/meta-st-stm32mp/recipes-graphics/drm/libdrm_2.4.100.bbappend
# End
############################
I then needed to create a bbappend for linux-stm32mp_5.4.bb in my layer
BB_STRICT_CHECKSUM = "0"
It was a hacky work around and I need to find the md5 for the linux.tar it was faulting on.
Then call the standard:
DISTRO=openstlinux-weston MACHINE=stm32mp1 source layers/meta-st/scripts/envsetup.sh
bitbake-layers add-layer ../layers/meta-my-test-layer/
bitbake st-image-weston
This gives me an image I can deploy on the dk2 but using my own dts is a really painful process around the optee where I had to copy lots of files by hand to make it work. I'm trying to modify the recipes so this is an automated process and will report back when I get a robust solution
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-06-27 3:20 AM
Hi @EButl.1
Is there any update on this: "using my own dts is a really painful process around the optee where I had to copy lots of files by hand to make it work. I'm trying to modify the recipes so this is an automated process and will report back when I get a robust solution"
I am trying to building the image with the cubemx files generated for our SOM board but failing due to the above mentioned similar issue.
Thanks