cancel
Showing results for 
Search instead for 
Did you mean: 

STM32MP133C Ethernet/PHY issue

Aerokii
Associate III

Hello! I'm working on bringing up a bare-metal STM32MP133C bare-metal on the dev kit from DIGI, using the HAL layer from ST. The problem I'm running in to is we're getting stuck on HAL_ETH_Init as when we enable the MAC clock, DMAMR's 0 bit (the reset bit) is stuck at 1, causing a timeout. 

 

From reading the reference manual, all related clocks need to be enabled for the reset to work, so I'm operating under the assumption there's a clock issue. I've initialized/configured the peripheral clock for PLL4, I'm enabling the relevant GPIO clocks, along with the ethernet clocks ETH1CK, ETH1TX, ETH1RX, and ETH1MAC. This leads me to believe the issue may be with the PHY clock. As we're using the Marvell PHY that comes with the board, I've (attempted) to set it so the PHY uses PLL4 by changing the appropriate bits in syscfg's PMCSETR. 

 

I figured that would be enough to get it all going... but it still seems I'm missing something. I've tried generating the code from CubeMX to see if it was a GPIO issue with no luck. I've attached the (very rough) file I'm working out of at present.

 

Thanks in advance for any support provided!

10 REPLIES 10

Looks like it was a combination of issues. I've been able to get it moving by setting up syscfg, confirming/adding some GPIOs that were not included in either CubeMX or anywhere obvious in the Digi dtsi file, and as recommended, setting PI2. For those who follow in my footsteps, I found this repo helpful as well: GitHub - Oryx-Embedded/CycloneTCP: Dual IPv4/IPv6 Stack.

 

Thanks much for your assistance!