2024-07-30 8:20 AM
Hello,
I am trying to set up a web browser on my STM32MP157F-DK2 board.
Following https://wiki.st.com/stm32mpu/wiki/How_to_install_a_simple_web_browser.
I tried:
root@stm32mp15-disco:~# apt-get install qt-wpe-simple-browser
Reading package lists... Done
Building dependency tree... Done
Reading state information... Done
E: Unable to locate package qt-wpe-simple-browser
apt-get update was successful.
Using apt-search doesn't locate the package.
However, source.list file seems properly configured.
Any clue would be appreciated.
Best Regards,
Vincent
Solved! Go to Solution.
2024-08-02 6:46 AM
Hello @Jean-Marc B ,
Thanks for your help.
I have successfully executed the different steps you have listed and obtained the same result.
Now if i try to compile the application
bitbake qt-wpe-simple-browserI obtain the following error during the do_configure step:
| WARNING: No QPA platform plugin enabled! This will
| produce a Qt that cannot run GUI applications.
| See "Platform backends" in the output of --help.
|
| ERROR: Feature 'opengl-desktop' was enabled, but the pre-condition '(config.win32 && !config.winrt && !features.opengles2 && (config.msvc || libs.opengl))
| || (!config.watchos && !config.win32 && !config.wasm && libs.opengl)' failed.
|
| ERROR: The OpenGL functionality tests failed!
| You might need to modify the include and library search paths by editing QMAKE_INCDIR_OPENGL[_ES2],
| QMAKE_LIBDIR_OPENGL[_ES2] and QMAKE_LIBS_OPENGL[_ES2] in the mkspec for your platform.
| WARNING: exit code 3 from a shell command.
ERROR: Task (/home/vincent/Documents/03_DEV/Distribution_package/layers/meta-qt5/recipes-qt/qt5/qtbase_git.bb:do_configure) failed with exit code '1'
NOTE: Tasks Summary: Attempted 3168 tasks of which 3163 didn't need to be rerun and 1 failed.
NOTE: Writing buildhistory
NOTE: Writing buildhistory took: 2 seconds
Summary: 1 task failed:
/home/vincent/Documents/03_DEV/Distribution_package/layers/meta-qt5/recipes-qt/qt5/qtbase_git.bb:do_configureThe full log is attached to the post.
Best Regards,
Vincent
2024-08-02 8:02 AM
Hello @Jean-Marc B ,
Thanks the advice. I have followed the different steps and obtained the same result.
However, when I try to compile the application, I obtain the following error (the full log is attached)
$ bitbake qt-wpe-simple-browser...
|
| WARNING: No QPA platform plugin enabled! This will
| produce a Qt that cannot run GUI applications.
| See "Platform backends" in the output of --help.
|
| ERROR: Feature 'opengl-desktop' was enabled, but the pre-condition '(config.win32 && !config.winrt && !features.opengles2 && (config.msvc || libs.opengl))
| || (!config.watchos && !config.win32 && !config.wasm && libs.opengl)' failed.
|
| ERROR: The OpenGL functionality tests failed!
| You might need to modify the include and library search paths by editing QMAKE_INCDIR_OPENGL[_ES2],
| QMAKE_LIBDIR_OPENGL[_ES2] and QMAKE_LIBS_OPENGL[_ES2] in the mkspec for your platform.
| WARNING: exit code 3 from a shell command.
ERROR: Task (/home/vincent/Documents/03_DEV/Distribution_package/layers/meta-qt5/recipes-qt/qt5/qtbase_git.bb:do_configure) failed with exit code '1'
NOTE: Tasks Summary: Attempted 3168 tasks of which 3163 didn't need to be rerun and 1 failed.
NOTE: Writing buildhistory
NOTE: Writing buildhistory took: 2 secondsBest regards,
Vincent
2024-08-02 8:21 AM
Hi @VLacr.1
This is more or less related to Qt and I am not a Qt expert!
I would recommend to switch to the ecosystem 5.0.0 which has the default meta-qt5 integration and add the meta-webkit layer. Perhaps it would help you.
Best regards,
--JM
2024-08-02 8:26 AM
Hello @Jean-Marc B ,
Ok.
Thanks to the previous step, I have built an image with WPE and COG. I can use the latest as a web browser (instead of qt-simple-web-browser) so it is fine for my initial need.
I then think we can close the ticket. Thanks again for your help.
Best Regards,
Vincent
2024-10-15 10:35 PM
Hi @Jean-Marc B @VLacr.1
I used the same method and complete the build process without error , but when i launch the qt-wpe-simple-browser, it will give me the error, wpewebkit-qtwpe-qml-plugin not installed
can you please let me know where i am missing ,
then i include this line into local.conf
MAGE_INSTALL:append = " wpewebkit-qtwpe-qml-plugin qt-wpe-simple-browser"
again i attempt to build , but unsuccessful on do_rootfs, and error " wpewebkit-qtwpe-qml-plugin dev not found no such file"
please let me know any other method to do this ?