2020-10-26 3:18 PM
Hello everybody,
Here is my problem. I am using the buildroot distro instead of OpenSTLinux and want to
connect my STM32 via ethernet using SSH. I use MobaXterm as remote control software.
P.s After a system boot I get the following response although the ethernet LEDs are not blinking
buildroot login: [ 4.237860] stm32-dwmac 5800a000.ethernet eth0: Link
is Up - 1Gbps/Full - flow control rx/tx
[ 4.251707] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes readyAfter ifconfig -a I get the following response:
eth0 Link encap:Ethernet HWaddr 00:80:E1:42:6B:16
inet addr:192.168.8.45 Bcast:192.168.8.255
Mask:255.255.255.0
inet6 addr: fe80::280:e1ff:fe42:6b16/64 Scope:Link
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:107 errors:0 dropped:0 overruns:0 frame:0
TX packets:11 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:10299 (10.0 KiB) TX bytes:866 (866.0 B)
Interrupt:60 Base address:0x8000This configuration was generated manually by etc / network and then nano
Interfaces where it says:
auto lo
iface lo inet loopback
# Configure eth0 with static IP
auto eth0
iface eth0 inet static
address 192.168.8.45
network 192.168.8.0
netmask 255.255.255.0
broadcast 192.168.8.255
gateway 192.168.8.1
dns-nameservers 192.168.8.1
# Configure eth0 with dhcp IP
# auto eth0
# iface eth0 inet dhcpMy setup is made like this. My PC is connected to WiFi through one Huawei Giga Cube and the STM32 are connected to my PC by a Ethernet cable.
If I go into Windows cmd and use ipconfig / all then I get the following output:
Windows IP Configuration
Host Name . . . . . . . . . . . . : ...
Primary Dns Suffix . . . . . . . :
Node Type . . . . . . . . . . . . : Broadcast
IP Routing Enabled. . . . . . . . : No
WINS Proxy Enabled. . . . . . . . : No
Ethernet adapter Ethernet:
Media State . . . . . . . . . . . : Media disconnected
Connection-specific DNS Suffix . :
Description . . . . . . . . . . . : Intel(R) Ethernet Connection (6)
I219-V
Physical Address. . . . . . . . . : 48-2A-E3-50-1B-76
DHCP Enabled. . . . . . . . . . . : Yes
Autoconfiguration Enabled . . . . : Yes
Unknown adapter NordLynx:
Connection-specific DNS Suffix . :
Description . . . . . . . . . . . : NordLynx Tunnel
Physical Address. . . . . . . . . :
DHCP Enabled. . . . . . . . . . . : No
Autoconfiguration Enabled . . . . : Yes
Link-local IPv6 Address . . . . . :
fe80::8df6:2969:45f4:3946%14(Preferred)
Autoconfiguration IPv4 Address. . : 169.254.57.70(Preferred)
Subnet Mask . . . . . . . . . . . : 255.255.0.0
Default Gateway . . . . . . . . . :
DNS Servers . . . . . . . . . . . : fec0:0:0:ffff::1%1
fec0:0:0:ffff::2%1
fec0:0:0:ffff::3%1
NetBIOS over Tcpip. . . . . . . . : Enabled
Ethernet adapter Ethernet 2:
Connection-specific DNS Suffix . :
Description . . . . . . . . . . . : Realtek USB GbE Family Controller
Physical Address. . . . . . . . . : 00-E0-4C-68-2E-FD
DHCP Enabled. . . . . . . . . . . : Yes
Autoconfiguration Enabled . . . . : Yes
Link-local IPv6 Address . . . . . :
fe80::ddff:5546:f233:2654%19(Preferred)
Autoconfiguration IPv4 Address. . : 169.254.38.84(Preferred)
Subnet Mask . . . . . . . . . . . : 255.255.0.0
Default Gateway . . . . . . . . . :
DHCPv6 IAID . . . . . . . . . . . : 419487820
DHCPv6 Client DUID. . . . . . . . :
00-01-00-01-24-C3-57-40-48-2A-E3-50-1B-76
DNS Servers . . . . . . . . . . . : fec0:0:0:ffff::1%1
fec0:0:0:ffff::2%1
fec0:0:0:ffff::3%1
NetBIOS over Tcpip. . . . . . . . : Enabled
Ethernet adapter Ethernet 4:
Media State . . . . . . . . . . . : Media disconnected
Connection-specific DNS Suffix . :
Description . . . . . . . . . . . : TAP-NordVPN Windows Adapter V9
Physical Address. . . . . . . . . : 00-FF-E3-A4-9C-52
DHCP Enabled. . . . . . . . . . . : Yes
Autoconfiguration Enabled . . . . : Yes
Ethernet adapter Ethernet 5:
Connection-specific DNS Suffix . :
Description . . . . . . . . . . . : VirtualBox Host-Only Ethernet
Adapter
Physical Address. . . . . . . . . : 0A-00-27-00-00-1A
DHCP Enabled. . . . . . . . . . . : No
Autoconfiguration Enabled . . . . : Yes
Link-local IPv6 Address . . . . . :
fe80::b4ff:a90a:c8d:424a%26(Preferred)
IPv4 Address. . . . . . . . . . . : 192.168.206.1(Preferred)
Subnet Mask . . . . . . . . . . . : 255.255.255.0
Default Gateway . . . . . . . . . :
DHCPv6 IAID . . . . . . . . . . . : 1024065575
DHCPv6 Client DUID. . . . . . . . :
00-01-00-01-24-C3-57-40-48-2A-E3-50-1B-76
DNS Servers . . . . . . . . . . . : fec0:0:0:ffff::1%1
fec0:0:0:ffff::2%1
fec0:0:0:ffff::3%1
NetBIOS over Tcpip. . . . . . . . : Enabled
Unknown adapter LAN-Verbindung:
Media State . . . . . . . . . . . : Media disconnected
Connection-specific DNS Suffix . :
Description . . . . . . . . . . . : TAP-Windows Adapter V9
Physical Address. . . . . . . . . : 00-FF-6A-9C-8E-76
DHCP Enabled. . . . . . . . . . . : Yes
Autoconfiguration Enabled . . . . : Yes
Wireless LAN adapter LAN-Verbindung* 1:
Media State . . . . . . . . . . . : Media disconnected
Connection-specific DNS Suffix . :
Description . . . . . . . . . . . : Microsoft Wi-Fi Direct Virtual
Adapter #3
Physical Address. . . . . . . . . : 24-EE-9A-7C-90-D0
DHCP Enabled. . . . . . . . . . . : Yes
Autoconfiguration Enabled . . . . : Yes
Wireless LAN adapter LAN-Verbindung* 12:
Media State . . . . . . . . . . . : Media disconnected
Connection-specific DNS Suffix . :
Description . . . . . . . . . . . : Microsoft Wi-Fi Direct Virtual
Adapter #4
Physical Address. . . . . . . . . : 26-EE-9A-7C-90-CF
DHCP Enabled. . . . . . . . . . . : Yes
Autoconfiguration Enabled . . . . : Yes
Wireless LAN adapter WLAN:
Connection-specific DNS Suffix . :
Description . . . . . . . . . . . : Intel(R) Wireless-AC 9560 160MHz
Physical Address. . . . . . . . . : 24-EE-9A-7C-90-CF
DHCP Enabled. . . . . . . . . . . : Yes
Autoconfiguration Enabled . . . . : Yes
Link-local IPv6 Address . . . . . :
fe80::ac7a:f511:a7ab:a012%23(Preferred)
IPv4 Address. . . . . . . . . . . : 192.168.8.124(Preferred)
Subnet Mask . . . . . . . . . . . : 255.255.255.0
Lease Obtained. . . . . . . . . . : Monday, October 26, 2020 9:45:02
PM
Lease Expires . . . . . . . . . . : Tuesday, October 27, 2020
10:28:23 PM
Default Gateway . . . . . . . . . : 192.168.8.1
DHCP Server . . . . . . . . . . . : 192.168.8.1
DHCPv6 IAID . . . . . . . . . . . : 287633050
DHCPv6 Client DUID. . . . . . . . :
00-01-00-01-24-C3-57-40-48-2A-E3-50-1B-76
DNS Servers . . . . . . . . . . . : fe80::5625:eaff:fe6f:3ce6%23
192.168.8.1
NetBIOS over Tcpip. . . . . . . . : Enabled
Ethernet adapter Bluetooth-Netzwerkverbindung:
Media State . . . . . . . . . . . : Media disconnected
Connection-specific DNS Suffix . :
Description . . . . . . . . . . . : Bluetooth Device (Personal Area
Network)
Physical Address. . . . . . . . . : 24-EE-9A-7C-90-D3
DHCP Enabled. . . . . . . . . . . : Yes
Autoconfiguration Enabled . . . . : Yes
Ethernet adapter vEthernet (Default Switch):
Connection-specific DNS Suffix . :
Description . . . . . . . . . . . : Hyper-V Virtual Ethernet Adapter
Physical Address. . . . . . . . . : 00-15-5D-65-E6-15
DHCP Enabled. . . . . . . . . . . : No
Autoconfiguration Enabled . . . . : Yes
Link-local IPv6 Address . . . . . :
fe80::74c4:a88f:e305:e735%22(Preferred)
IPv4 Address. . . . . . . . . . . : 192.168.238.241(Preferred)
Subnet Mask . . . . . . . . . . . : 255.255.255.240
Default Gateway . . . . . . . . . :
DHCPv6 IAID . . . . . . . . . . . : 369104221
DHCPv6 Client DUID. . . . . . . . :
00-01-00-01-24-C3-57-40-48-2A-E3-50-1B-76
DNS Servers . . . . . . . . . . . : fec0:0:0:ffff::1%1
fec0:0:0:ffff::2%1
fec0:0:0:ffff::3%1
NetBIOS over Tcpip. . . . . . . . : Enabled
Ethernet adapter vEthernet (WSL):
Connection-specific DNS Suffix . :
Description . . . . . . . . . . . : Hyper-V Virtual Ethernet Adapter
#2
Physical Address. . . . . . . . . : 00-15-5D-3A-2A-A7
DHCP Enabled. . . . . . . . . . . : No
Autoconfiguration Enabled . . . . : Yes
Link-local IPv6 Address . . . . . :
fe80::2165:e63f:cd0d:3e86%80(Preferred)
IPv4 Address. . . . . . . . . . . : 172.18.18.17(Preferred)
Subnet Mask . . . . . . . . . . . : 255.255.255.240
Default Gateway . . . . . . . . . :
DHCPv6 IAID . . . . . . . . . . . : 1342182749
DHCPv6 Client DUID. . . . . . . . :
00-01-00-01-24-C3-57-40-48-2A-E3-50-1B-76
DNS Servers . . . . . . . . . . . : fec0:0:0:ffff::1%1
fec0:0:0:ffff::2%1
fec0:0:0:ffff::3%1
NetBIOS over Tcpip. . . . . . . . : EnabledI hope that you can help me. Thank you all
2020-11-05 7:17 AM
Hi @SigmaPrime ,
Be aware that ST is not supporting buildroot solution directly, but only through some partner ( eg Bootlin) .
I suggest to have a look in our wiki , in case an article may guide you in the right direction, else try to get help from partner community.
Olivier
2020-11-05 7:27 AM
Thank you for your response.
I would say that they are not serious when responding to people. I managed to resolve the solution alone after multiple tries.
It appeared that my system configuration wasn't correct and that some packages were missing. I had to contact Rasp community to get the right info.
Buildroot forum is messy and when I want to upload multiple files with a modest size I can't do that so explaining my situation is really difficult when turning to them.
2020-11-05 10:18 PM
Hi,
for people wanting to start using buildroot for the STM32MP1 there is a GitHub Repo with a buildroot example for the STM32MP1. I'm pretty sure it doesn't contain a ssh packet at the start but you can easily use this as a starting point and activate something like dropbear. Helped me at the start using buildroot a lot besides some Bootlin blog articles.
Github repo:
https://github.com/schenkmi/buildroot-op-tee-stm32mp1
Cheers
2020-11-06 1:45 AM
Thank you gonna check it out