STM32 MPUs Boards and hardware tools

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

kmsdrm dynamic loading support

Hi, What mean kmsdrm no support dynamic loading ? But for example X11 can be dynamic loaded.I check this when try build SDL, but are there some another options to check dynamic loading in system ?Adrian

Adrian1 by Associate III
  • 763 Views
  • 1 replies
  • 0 kudos

How to Flash yocto image in STM32MP157A-DK1

Hello, We have a custom board with STM32MP157A series and we need to launch our image using EMMC boot.Actually we had an custom board with same processor but it was booting only with SD card as there is no EMMC boot in that.So I want to know how to...

Smedi by Associate II
  • 1030 Views
  • 3 replies
  • 0 kudos

Resolved! How to add program to autostart?

Hi, how to add program to autostart in OpenSTLinux ?I tried adding initialization script to /etc/init.d and creating .desktop file in ~/.config/autostart directory, but nothing works.I will be very gratefull, if somebody could help me.

La1 by Associate III
  • 2554 Views
  • 8 replies
  • 0 kudos

STM32MP151A custom board with eMMC sometimes go to DFU on power-up. Need help to write OTP word 3.

Hi. I've made a custom board very similar to stm32mp157c-DK2 BUT with STM32MP151A and ONLY eMMC (on SDMMC2 standard MUX) as flash device (no NOR, no QUADSPI, no SD). I built all necessary files with the help of CubeMX program and all works good EXCE...

GCici by Associate II
  • 1660 Views
  • 7 replies
  • 0 kudos