STM32 MPUs Boards and hardware tools

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Power Consumption with only the M4 running

We are using a STM32MP157A-DK1 and try to reduce power consumption.1) When A7 and M4 are running we measure around 300mA.2) When A7 is in Suspend-To-Mem and the M4 is still running we measure around 80mA.3) When the M4 also enters standby mode the po...

Daniel S. by Associate III
  • 1617 Views
  • 5 replies
  • 1 kudos

Resolved! Mistake in STM32MP1-DK2 schematics?

Hi all.The en.MB1272-DK2-C01_Schematic.pdf states thatARD_A0 : PF14 -> ADC1_IN0ARD_A1 : PF13 -> ADC1_IN1ARD_A2 : ANA0 -> ADC2_IN6ARD_A3 : ANA1 -> ADC2_IN2I've spend quite some time to figure out that this is wrong and the correct pinout is:ARD_A0...

dimtass by Associate II
  • 778 Views
  • 1 replies
  • 2 kudos

Resolved! How do I configure additional rootfs(additional Directory, more Package like as lighttpd)?

Hello everyone.​I am modifying the distribution packages of 157C-DK2 and 157C-EV1 for my project.​When I previously configured my rootfs using buildroot and debian-jessie, I proceeded as follows(other boards).Packages that can be configured using bui...

0693W000003PiZCQA0.png
SPark.15 by Associate II
  • 2040 Views
  • 4 replies
  • 0 kudos

Resolved! STPMIC1 efficiency at low load

Dear all, I am looking to use the STPMIC1 in one new STM32MP15x design which will spend most of this time in standby mode. I am looking for STPMIC1 buck efficiency at light load (~1mA). In the datasheet there is numbers only for 150mA, 750mA and 1A. ...

PGE by Associate III
  • 982 Views
  • 2 replies
  • 0 kudos