STM32 MPUs Boards and hardware tools

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Pinout/Functionality between STM32MP1 devices and development boards, are they mostly similar?

Hello,I would like to embark on a project for a custom board with the STM32MP157DAB1 and I am referencing the STM32MP15-DISCO schematic from ST which uses the STM32MP157CAC3.My Question: How do I translate between the functionality of the pins?From o...

0693W00000Hqit7QAB.png
daded.1 by Associate II
  • 1375 Views
  • 3 replies
  • 0 kudos

Resolved! How to enter DDR interactive mode by defining CONFIG_STM32MP1_DDR_INTERACTIVE ?

I am using stm32MP157F-DK eval board (on windows) and I would like to try the DDR testing tool on cubeMX. But this is my first time trying to do so - I try to follow steps in "U-Boot SPL: DDR interactive mode" (url: https://wiki.st.com/stm32mpu/wiki/...

Resolved! Image install to emmc using sd card

Hello GuysI'm using a157-EV1 board and my custom board.Both board have sd card slot and emmc. And possible of linux install to sd card and emmc.Anyway if built images using STM32_Programmer_CLI in Ubuntu environment can be install on the board accord...

SPark.15 by Associate II
  • 4230 Views
  • 5 replies
  • 0 kudos

Compilation error while rebuild kernel

Hi hope you're well. I got stuck on part 6.Compile kernel source code->Compile and install on the current source code directory->make ARCH=arm uImage vmlinux dtbs LOADADDR=0xC2000040 giving an error as below. Thanks in advance! CC     drivers/usb/dwc...

MKana.1 by Associate II
  • 2127 Views
  • 8 replies
  • 0 kudos