cancel
Showing results for 
Search instead for 
Did you mean: 

How to format input data to import in NanoEdge AI Studio

Pierre Guiglion
ST Employee

In NanoEdge AI Studio v3, sensor data can be imported either from file, or "live" from a data logger via serial (USB) port. In both cases, the data format is the same. 

There are 3 cases to distinguish, depending on which project type is selected in NanoEdge AI Studio.

Check the corresponding sections of the NanoEdge AI Studio documentation:

  1. General rules: anomaly detection and classification projects (1-class or n-class)
  2. Variant: extrapolation projects
  3. Exception: Multi-sensor (anomaly detection projects only)

Another option for importing data is to use the native Datalogger feature (only for STEVAL-STWINKT1B), which captures sensor data in .dat format, ready to be imported in the Studio, and automatically converted into Studio-compatible format.

Version history
Last update:
‎2025-08-01 1:32 AM
Updated by:
Contributors