FAQ: Default State of STM32H7 switches connecting Pxy_C and Pxy pads
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Email to a Friend
- Printer Friendly Page
- Report Inappropriate Content
2021-01-05 7:52 AM - edited 2025-01-07 9:55 AM
What is the state after reset of STM32H7 analog switches between Pxy_C and Pxy pins/balls?
The Reference Manual RM0399 Rev 3 (page 584) gives a figure as the one below , but not all Pxy_C and Pxy are accessible depending on the STM32H7 package.
The default state of the analog switches can be deduced from the STM32H7 package and can be read with a debugger.
1. Rules
- GPIOs are in analog mode during and just after reset (except the debug pins in alternate function mode after reset).
- But the digital alternate functions are accessible after reset whatever the package.
2. Default state
According to these rules, the default state of the switches depends on the package:
- If both Pxy and Pxy_C are available, the corresponding switch that connects the two internal pads is open by default.
- The alternate functions are accessible through Pxy pin/ball while the ADC input is available through Pxy_C pin/ball.
- If only Pxy is available, the switch is open by default.
- The alternate functions are accessible through Pxy pin/ball. To use the ADC connected to the internal pad Pxy_C, the switch shall be closed. In this case, the other functions of the Pxy pin/ball are no more accessible.
- If only Pxy_C is available, the switch is closed by default.
- The alternate functions are accessible through Pxy_C pin/ball. To use the ADC connected to the internal pad Pxy_C, the switch shall be opened.
3. SYSCFG peripheral mode configuration register (SYSCFG_PMCR)
The switch state can be read/modified in SYSCFG_PMCR.PxySO (Pxy Switch Open):
0: Analog switch closed (pads are connected through the analog switch)
1: Analog switch open (2 separated pads)
At this point, the datasheet is needed to know which pins are available on the STM32H7 package (pinout/ballout figure and pin/ball definition table).
The value of this SYSCFG_PMCR register can also be read in a debugger (after having enabled the clock by __HAL_RCC_SYSCFG_CLK_ENABLE()).
4. Examples