cancel
Showing results for 
Search instead for 
Did you mean: 

STM32WLE5 + USART on LSE in STOP2 mode

MLe M.1
Associate III

Hello,

From STM32CubeMx we can see that USART1 can be drived from LSE. LSE is active in Stop mode2.

From datasheet, USART1 is off in stop mode 2.

Is it sure that USART1 can not work from Stop mode 2 with low datarate?

Best regards

Michel

4 REPLIES 4
Peter BENSCH
ST Employee

Correct, none of the USARTs can operate in STOP 2, as you can read in the datasheet, table 8. The LPUART was developed for this case, and it can operate in STOP 2.

Hope that answers your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

@Peter BENSCH wrote:

The LPUART was developed for this cases


@MLe M.1  the clue is in the name, "LPUART" - the "LP" stands for Low Power 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
MLe M.1
Associate III

what is the maximum bps of LPUART1 using LSE?

I would like to have a 2nd LPUART .....