cancel
Showing results for 
Search instead for 
Did you mean: 

STM32WB55 Memory Layout

ROost.1
Associate

Hi,

I am new to the STM32WB range. I need to use the 1MB flash version in a project, But I am struggling a bit to understand the flash layout.

I read that the first 6 Sectors are to be used my the OTA application. It seems like settings should go directly after that (say one sector). Then you can place your code.

It is stated that the CPU2 application is at the end of flash. I cant seem to find any actual specifications on the exact location (or how big it is).

And does the code for CPU2 actually live on the same flash space?

I need to work out my boundaries. But it feels like i am missing some info that I dont seem to be getting from the docs.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0