2020-01-28 5:12 AM
Hello everyone,
I would like to use the Uart over BLE with the STM32WB55.
I'm not very familiar with BLE, but as I understood for now, Uart over BLE is not a Bluetooth SIG standard, but people have been developing custom services for it.
I couldn't find any example with the STM32WB55, does any have one with that?
I'm a looking for what is called a GATT server ?
Moreover, in STM32_WPAN middleware, I could find theses UUIDs. They seem to be related with my need but I'm not sure how to use it.
/* Custom Services*/
/* UUIDs for data transfer service */
#define DATA_TRANSFER_SERVICE_UUID (0xFE80)
#define DATA_TRANSFER_TX_CHAR_UUID (0xFE81)
#define DATA_TRANSFER_RX_CHAR_UUID (0xFE82)Best regards,
Rico
Solved! Go to Solution.
2020-01-28 6:27 AM
By UART do you mean a link over BLE?
We have a project here under STM32Cube_FW_WB_V1.4.0\STM32Cube_FW_WB_V1.4.0\Projects\P-NUCLEO-WB55.Nucleo\Applications\BLE\BLE_CableReplacement which emulates a cable connection to use as a Point-to-Point communication.
2020-01-28 6:27 AM
By UART do you mean a link over BLE?
We have a project here under STM32Cube_FW_WB_V1.4.0\STM32Cube_FW_WB_V1.4.0\Projects\P-NUCLEO-WB55.Nucleo\Applications\BLE\BLE_CableReplacement which emulates a cable connection to use as a Point-to-Point communication.
2020-01-28 6:34 AM
Hello Remi,
yes that's what I mean, I want to do a kind of terminal on the WB55 side, and on a smartphone be able to send custom frames.
Thank you for your answer, I'm going to see the project you mentionned, when I saw it's name I didn't understand it in that way ;)
Regards,
Eric