cancel
Showing results for 
Search instead for 
Did you mean: 

I'd like details on the modulation scheme used by STM32wb55 BLE chip for ETSI EN 300 328 approval.

RWill.4
Associate

Hi,

I'm taking an STM32wb55 based PCB through CE testing. The test house require the following information which I haven't got.

Modulation scheme

Duty cycles

Channel hopping

Worst case operational modes

Transmit operational modes

Medium Utilization

Any information would be helpful.

Rhydian

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Remi QUINTIN
ST Employee

What type of info regarding Duty Cycle are you looking for?

>Worst case operational modes

Dp you mean in a noisy environment with blockers inside and outside the BLE band?

Remi QUINTIN
ST Employee

For the CE certification for BLE devices, you must be compliant with EN 300 328 V2.2.2 :

Modulation scheme GFSK modulation width 2MHz

Duty cycles -> 98%

Channel hopping No -> DSSS

Worst case operational modes 2MHz

Transmit operational modes Permanent with modulation

Medium Utilization No