cancel
Showing results for 
Search instead for 
Did you mean: 

Can't discover STM32WB55 GATT Server after running p2pServer project from firmware.

RBech.1
Associate

Hello,

I am using STM32 Cube Ide and I am just getting started with the STM32 WB55 board. I tried running the p2p Server project from the firmware package but I can't see the board neither on nrf Connect application or ST BLE Sensor app. Does anyone has the same problem ?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Remi QUINTIN
ST Employee

​Did you try to load the BLE_p2pServer_reference.hex file located  under the

STM32Cube_FW_WB_V1.10.0\Projects\P-NUCLEO-WB55.Nucleo\Applications\BLE\BLE_p2pServer\Binary directory.

Then use the ST BLE sensor mobile application  to detect it and connect to it.

This would ensure your board is OK.