cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7 JPEG encoder MCU blocks - corrupted JPEG image

rob-bits
Associate II

I have an issue to understand the MCU blocks for JPEG encoder. I have an stm32h743 MCU which is connected to a video decoder with dcmi interface. In ram I have the captured 8-bit ITU-R BT.656 YCrCb 4:2:2 output. Saving the captured data from ram to a debug file, I can see the image is captured properly. The byte stream looks like: Cb0-1, Y0,Cr0-1, Y1, Cb2-3, Y2, CR2-3, Y3 .... total 720Y and 360CB and 360 CR, total 1440 bytes + 8 byte blanking per line. And I have 240 lines so the resolution that I am capturing is 720x240.

As described in the AN4996, each 4:2:2 MCU contains 256 bytes organized as two 8×8 Y blocks plus one 8×8 Cb block plus one 8×8 Cr block. For a 720×240 image, I should need 45 horizontal MCUs × 30 vertical MCUs = 1,350 total MCUs. My confusion is the two Y blocks. I implemented the two Y blocks as:

Y1 first row:
y0, y1 ... y7
Y1 second row:
y16, y17...y23
Y2 first row:
y8, y9, ... y15
Y2 second row:
y24, y25 .. y31
Is this correct?

So Y1 contains the first 8 pixel columns, and the Y2 contains the second 8 pixel columns?

Here is my code that processes the ycrcb byte stream:

#define MCU_BLOCK_ROWS 8  // 8x8 block = 64 bytes
#define MCU_BLOCK_COLS 8  // 8x8 block = 64 bytes
#define MCU_BLOCK_SIZE (MCU_BLOCK_ROWS * MCU_BLOCK_COLS)  // 8x8 block = 64 bytes
#define MCU_SIZE 256
__attribute__((section(".axiram"))) static uint8_t mcuBuffers[2][MCU_SIZE]; 
 
static void ExtractMcuToBuffer(uint8_t* src, uint8_t* dest, uint32_t block_cnt) {
    uint8_t* y1 = dest;        // Y block 1
    uint8_t* y2 = dest + 64;   // Y block 2
    uint8_t* cb = dest + 128;  // Cb block
    uint8_t* cr = dest + 192;  // Cr block
  // 720x240 → 720 / 16 bytes, 240/8 bytes -> 45x30 = 1350 MCUs
    uint32_t mcuRowIdx = block_cnt / 45;
    uint32_t mcuColIdx = block_cnt - (mcuRowIdx * 45);
    //the number of bytes in one line, left offset + right offset + width = 1576,
    // 4 byte was 1 pixel with this offset
    uint32_t lineOffset = 1448; //how much bytes are in a line -> determined by trial and error, this is how many samples are captured by dcmi, including blanking
    // Optimized MCU extraction for 4:2:2 UYVY format
    uint32_t rowIdx = 0;
    uint32_t colIdx = 0;
    uint32_t byteOffset = (lineOffset * MCU_BLOCK_ROWS * mcuRowIdx ) //we need to skip MCU_BLOCK_ROWS of lines times mcuRowIdx
    		+ (lineOffset * 0) //we need to do offset lines based on the row idx, in the begining we are at 0 line, for second line of MCU we need to get the second line of the ycrcb buffer
			+ mcuColIdx * 32; // we need an offset based on in which MCU block we are working on, 0, 1... One MCU block consist of 32 bytes,16xY, 8xCr and 8xCb 32 x 45 -> 1440 bytes, max(mcuColIdx) = 44, 32 * 44 + 32 -> 1440 samples
    uint32_t* crycby = (uint32_t*)&src[byteOffset];
    for(int i = 0; i < MCU_BLOCK_SIZE;i++) {
      
      uint8_t Y1 = (uint8_t) ((*crycby & 0x000000FF) >> 0);
      uint8_t Cr = (uint8_t) ((*crycby & 0x0000FF00) >> 8);
      uint8_t Y2 = (uint8_t) ((*crycby & 0x00FF0000) >> 16);
      uint8_t Cb = (uint8_t) ((*crycby & 0xFF000000) >> 24);
      crycby++; //increase four bytes in the address
      *cr++ = Cr;    // cr
      *cb++ = Cb;    // cb

      //building Y1
      if(colIdx < MCU_BLOCK_COLS/2) {
          *y1++ = Y1;     //yn
          *y1++ = Y2;    // yn+1
      } else {//building Y2
          *y2++ = Y1;     //yn
          *y2++ = Y2;    // yn+1
      }
      if(colIdx < MCU_BLOCK_COLS - 1) {
        colIdx++;
      } else { //here we switch line
        colIdx = 0;
        rowIdx++;
        byteOffset = (lineOffset * MCU_BLOCK_ROWS * mcuRowIdx ) +  rowIdx * lineOffset + mcuColIdx * 32;
        crycby = (uint32_t*)&src[byteOffset];
      }
    }
}

The block_cnt goes from 0 to 1349.

With this code, I got this jpeg image:

robbits_0-1750143337325.png

 

The file header, resolution looks okay, but the content is corrupted. And I am not sure why.

Any idea?

0 REPLIES 0