cancel
Showing results for 
Search instead for 
Did you mean: 

Print a string on TFT Display.

LACTIC
Associate II

I am using STM32F429ZI Nucleo Bord by using LTDC . I have already print a image on that by using this system peripheral but when I am going to print string on that it not print on screen. Please help .

my written code :--

 BSP_LCD_Init();

 BSP_LCD_LayerDefaultInit(LCD_BACKGROUND_LAYER,LCD_FRAME_BUFFER);

 BSP_LCD_SelectLayer(LCD_BACKGROUND_LAYER);

 BSP_LCD_Clear(LCD_COLOR_WHITE);

 //BSP_LCD_SetTextColor(LCD_COLOR_BLACK);

 BSP_LCD_DisplayStringAtLine(1,(uint8_t*)"hi");

 BSP_LCD_DisplayStringAtLine(5,(uint8_t*)"HELLO");

These API are in attached ".c and .h" file

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
LACTIC
Associate II

I am using inbuilt sram which start from 0x20000000 and lcd size is 320*240 and according to calculation required frame buffer size =2*( (320*240*2)/1024) { for 16bit } that is 300 (k byte).