cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L0 SPI CRC Error

tianchen
Associate II
Posted on April 25, 2015 at 01:18

Hi,

 

 

I modify the spi sample code but enable CRC function, however I always get CRCERR. I dont know the reason.

 

 

Here is the initialization of SPI:

SPI2->CR1 |= SPI_BAUDRATEPRESCALER_256;

SPI2->CR1 &= ~SPI_CR1_CPOL;

SPI2->CR1 &= ~SPI_CR1_CPHA;

SPI2->CR1 &= ~SPI_CR1_BIDIMODE;

SPI2->CR1 |= SPI_CR1_CRCEN;

SPI2->CR1 &= ~SPI_CR1_RXONLY;

SPI2->CR1 |= SPI_CR1_SSM;

SPI2->CR1 |= SPI_CR1_SSI;

SPI2->CR1 &= ~SPI_CR1_LSBFIRST;

SPI2->CR1 |= SPI_CR1_MSTR;

SPI2->CR1 &= ~SPI_CR1_DFF;

  /* Configure : NSS management */

SPI2->CR2 |= SPI_CR2_SSOE;

  /* Configure : CRC Polynomial */

  SPI2->CRCPR = 0x07;  //reset value

Here is the Transmit function:

uint8_t SPI_Transmit(uint8_t *pData, uint16_t Size, uint32_t Timeout)

{

__IO uint16_t tmpreg;

uint8_t* pTxBuffPtr = pData;

uint16_t TxCount = Size;

  if(SPI_State == SPI_STATE_READY)

  {

    if((pTxBuffPtr == NULL ) || (TxCount == 0)) 

    {

      return  STATUS_ERROR;

    }

SPI_State = SPI_STATE_BUSY_TX;

    /* Reset CRC Calculation */

if(SPI2->CR1 & SPI_CR1_CRCEN)

{

SPI2->CR1 &= ~SPI_CR1_CRCEN;

SPI2->CR1 |= SPI_CR1_CRCEN;

}

    /* Check if the SPI is already enabled */ 

    if((SPI2->CR1 & SPI_CR1_SPE) != SPI_CR1_SPE)

    {

      /* Enable SPI peripheral */

      SPI2->CR1 |=  SPI_CR1_SPE;

    }

if(TxCount == 0x01)

{

SPI2->DR = *pTxBuffPtr++;

TxCount--;

}

while(TxCount > 0)

{

/* Wait until TXE flag is set to send data */

if(SPI_WaitOnFlagUntilTimeout(SPI_SR_TXE, RESET, Timeout) != STATUS_OK)

return STATUS_TIMEOUT;

}

SPI2->DR = *pTxBuffPtr++;

TxCount--;

}

/* Enable CRC Transmission */

if(SPI2->CR1 & SPI_CR1_CRCEN) 

{

SPI2->CR1 |= SPI_CR1_CRCNEXT;

}

    /* Wait until TXE flag is set to send data */

    if(SPI_WaitOnFlagUntilTimeout(SPI_SR_TXE, RESET, Timeout) != STATUS_OK)

    {

      return STATUS_TIMEOUT;

    }

    /* Wait until Busy flag is reset before disabling SPI */

    if(SPI_WaitOnFlagUntilTimeout(SPI_SR_BSY, SET, Timeout) != STATUS_OK)

    { 

      return STATUS_TIMEOUT;

    }

 

    /* Clear OVERUN flag in 2 Lines communication mode because received is not read */

    if((SPI2->CR1 & SPI_CR1_BIDIMODE) == 0)

    {

      tmpreg = SPI2->DR;

      tmpreg = SPI2->SR;

    }

SPI_State = SPI_STATE_READY;

    return STATUS_OK;

}

  else

  {

    return STATUS_BUSY;

  }

}

After call this function, CRCERR bit will be set.

 

I enable CRCNEXT bit after last data is written to the SPI_DR register.

 

It should be ok right?

 

What is the problem? Please help me.

 

Thank you.

#stm32 #crc #spi
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0