cancel
Showing results for 
Search instead for 
Did you mean: 

Working with STM32F407ZET6. What is the resolution time base of the tick interrupt that is driving the scheduler?

MSaik
Associate

Following a guide to view run-time statistics. The guide says to set up a hardware timer, "The timer used for collecting these statistics must use a higher resolution time base than the tick interrupt that is driving the scheduler, otherwise the statistics will be too inaccurate or even useless." I am wondering how fast the tick interrupt is

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1

SysTick is frequently 1ms (1KHz)

Shouldn't be too hard to look at your code and see what HAL_Init() and HAL_InitTick(), or overloaded, versions are actually doing..

/**
  * @brief This function configures the source of the time base.
  *        The time source is configured  to have 1ms time base with a dedicated 
  *        Tick interrupt priority.
  * @note This function is called  automatically at the beginning of program after
  *       reset by HAL_Init() or at any time when clock is reconfigured  by HAL_RCC_ClockConfig().
  * @note In the default implementation, SysTick timer is the source of time base. 
  *       It is used to generate interrupts at regular time intervals. 
  *       Care must be taken if HAL_Delay() is called from a peripheral ISR process, 
  *       The SysTick interrupt must have higher priority (numerically lower)
  *       than the peripheral interrupt. Otherwise the caller ISR process will be blocked.
  *       The function is declared as __weak  to be overwritten  in case of other
  *       implementation  in user file.
  * @param TickPriority Tick interrupt priority.
  * @retval HAL status
  */
__weak HAL_StatusTypeDef HAL_InitTick(uint32_t TickPriority)
{
  /* Configure the SysTick to have interrupt in 1ms time basis*/
  if (HAL_SYSTICK_Config(SystemCoreClock / (1000U / uwTickFreq)) > 0U)
  {
    return HAL_ERROR;
  }
 
  /* Configure the SysTick IRQ priority */
  if (TickPriority < (1UL << __NVIC_PRIO_BITS))
  {
    HAL_NVIC_SetPriority(SysTick_IRQn, TickPriority, 0U);
    uwTickPrio = TickPriority;
  }
  else
  {
    return HAL_ERROR;
  }
 
  /* Return function status */
  return HAL_OK;
}

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..