cancel
Showing results for 
Search instead for 
Did you mean: 

Why the stm32f103 CAN in the simulink can not distinguish

hongjin zeng
Associate
Posted on December 30, 2017 at 11:01

Hello everyone:

  I am a vehicle software engineer. Now I need to do a industry control project. I want to use stm32f103zdt6.First I configure the .ioc file and creat a simulink model and configure it.Second I drag the STM32_config block in the model and configure the block.Then I drag the CAN_IT block in the model,but I find the block can not read the ioc file's setting.In the ioc file I enable the CAN RX0 and SCE interrupt,but in the Simulink The CAN_IT block can not read it.I think this is a bug.Please fix the bug quickly.

#stm32-mat/target-matlab #simulink
1 REPLY 1
Posted on December 31, 2017 at 14:47

>>

I think this is a bug. Please fix the bug quickly.

There is a lesson here about being dependent on third-parties for meeting one's own deadlines. The other parties usually have different, and divergent, priorities.

For commercial work you should contact your local ST sales/support office, and work with an FAE

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..