cancel
Showing results for 
Search instead for 
Did you mean: 

Why one of the GPIOs (PB7), configured as output, is giving only 1.58V instead of 3.3V when it is set? I have the STM32L432KC nucleo.

xpp07
Senior
 
This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4

You have something else on the pin driving it low, and they are fighting? Check the schematic.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
xpp07
Senior

I don't have anything connected to the pin. I'm measuring with no load.

waclawek.jan
Super User

So you disconnected SB18?

JW

xpp07
Senior

I don't have the controller right now to check. But I'm almost sure that should be the case. Thank you. I should've paid more attention to the schematic in the user manual.