cancel
Showing results for 
Search instead for 
Did you mean: 

What is the difference between UART?

Carter Lee
Associate III
Posted on September 21, 2017 at 16:09

Dear all ST,

Now I'm trying to implement UART but I can't get receive all data at the time. this case need delay() to get all data..

So I've another difference way used in the same project, then it's works.

BTW, I can find the differences.

#example which is needed delay()  case .

int main(void)

{

////////////////////////////////////////////////////////////

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;//GPIO_PuPd_UP;

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

GPIO_Init(GPIOD, &GPIO_InitStructure);

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_11;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;//GPIO_PuPd_UP;

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

GPIO_Init(GPIOC, &GPIO_InitStructure);

GPIO_PinAFConfig(GPIOD, GPIO_PinSource5, GPIO_AF_USART2); // USART1_TX

GPIO_PinAFConfig(GPIOC, GPIO_PinSource11, GPIO_AF_USART3); // USART1_RX

USART_InitStructure.USART_BaudRate = 115200;

USART_InitStructure.USART_WordLength = USART_WordLength_8b;

USART_InitStructure.USART_StopBits = USART_StopBits_1;

USART_InitStructure.USART_Parity = USART_Parity_No;

USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;

USART_InitStructure.USART_Mode = USART_Mode_Rx ;

USART_Init(USART3, &USART_InitStructure);

USART_Cmd(USART3, ENABLE);

USART_InitStructure.USART_BaudRate = 115200;

USART_InitStructure.USART_WordLength = USART_WordLength_8b;

USART_InitStructure.USART_StopBits = USART_StopBits_1;

USART_InitStructure.USART_Parity = USART_Parity_No;

USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;

USART_InitStructure.USART_Mode = USART_Mode_Tx;

USART_Init(USART2, &USART_InitStructure);

USART_Cmd(USART2, ENABLE);

/////////////////////////////////////////////////////////////////////////////////

NVIC_InitStructure.NVIC_IRQChannel = USART3_IRQn;

NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0x00;

NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0x00;

NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

NVIC_Init(&NVIC_InitStructure);

USART_ITConfig(USART3, USART_IT_RXNE, ENABLE);

VS

Working good example.

int main(void)

{

RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOG, ENABLE);

RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);

RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG, ENABLE);

//RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE);

RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2, ENABLE);

//RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART3, ENABLE);

RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE);

RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD, ENABLE);

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5 | GPIO_Pin_6;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; 

GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; 

GPIO_Init(GPIOD, &GPIO_InitStructure);

GPIO_PinAFConfig(GPIOD, GPIO_PinSource5, GPIO_AF_USART2); // USART1_TX

GPIO_PinAFConfig(GPIOD, GPIO_PinSource6, GPIO_AF_USART2); // USART1_RX

USART_InitStructure.USART_BaudRate = 115200;

USART_InitStructure.USART_WordLength = USART_WordLength_8b;

USART_InitStructure.USART_StopBits = USART_StopBits_1;

USART_InitStructure.USART_Parity = USART_Parity_No;

USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;

USART_InitStructure.USART_Mode = USART_Mode_Tx | USART_Mode_Rx;

USART_Init(USART2, &USART_InitStructure);

USART_Cmd(USART2, ENABLE);

NVIC_InitStructure.NVIC_IRQChannel = USART2_IRQn;

NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0x00;

NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0x00;

NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

NVIC_Init(&NVIC_InitStructure);

/* Enable USART1 Receive and Transmit interrupts */

USART_ITConfig(USART2, USART_IT_RXNE, ENABLE);

Can you see the difference ?

What am I supposed to do to get the all data without delay at the first case?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0