cancel
Showing results for 
Search instead for 
Did you mean: 

What is Dual Address Mode in I2C Handle

Jennifer Liu
Associate
Posted on October 27, 2017 at 19:36

What is Dual Address Mode in I2C Handle? 

#i2c-addressing
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on October 28, 2017 at 09:47

Hello!

Dual Address mode is valid only in slave mode.

Dual Address mode in I2c handle can have two values, I2C_DUALADDRESS_DISABLE or enabled

When enabled(ENDUAL bit of I2C_OAR2 register is set) . OwnAddress2 (in same handle) used also as valid slave address for device regognition by the Master of I2C Bus.