cancel
Showing results for 
Search instead for 
Did you mean: 

view timers in the ride simulator

guyvo67
Associate II
Posted on March 20, 2009 at 07:24

view timers in the ride simulator

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
guyvo67
Associate II
Posted on May 17, 2011 at 13:07

Hi,

I tried to change several types (REVT6/8) of ST32 for the ride IDE. But al them shows only 4 timers in the peripheral view although I defined them in the conf file like this:

#define _TIM

#define _TIM1

#define _TIM2

#define _TIM3

#define _TIM4

#define _TIM5

#define _TIM6

#define _TIM7

#define _TIM8

Is this not possible in simulator or only with real target ?

(can't test it because I have only 4 timers on my target board)

Thanks

Guy