cancel
Showing results for 
Search instead for 
Did you mean: 

Vdd of STM32L100C-DISCO

kozlovdmn
Associate II
Posted on November 17, 2015 at 15:31

I have this board a couple of days. I am trying to blink LEDs. With green one it works fine, but with blue one it doesn't work.

I think the problem lies in the 2V VDD. LED works if it is supplied by external source. The pin state is changed according to code.

Does anybody have this board? Manual claims that VDD is 3.3V

UPD. Sorry for bothering you. It took only one day to slightly move JP2 to repair it. =))
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Amel NASRI
ST Employee
Posted on November 19, 2015 at 10:26

Hi Prog,

Great to hear that you fixed your problem and update us on this regard.

You have to refer to the board's user manual in such case anyway.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Posted on November 19, 2015 at 13:11

Most DISCO boards run the chips at 3.0V

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..