cancel
Showing results for 
Search instead for 
Did you mean: 

VCP Problems with HAL Libraries and the STM32F4 Discovery

mathias
Associate II
Posted on September 02, 2014 at 15:22

Hi everybody,

I have a problem with the VCP. I want to make a UART Connection between the STM-Board (STM32F4 Discovery) and my PC with the MicroUSB. Has anybody a working code for me. I know, I could use a UART Interface with a FTDI board, but I want to work with the MicroUSB.

With kind regards

Mathias
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on September 02, 2014 at 18:40

Has anybody a working code for me.

I've published working examples using the Standard Peripheral Library, and USB Firmware Library, for Cube/HAL you'll need to fish here, or [DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Java/AllItems.aspx]the forum it's being supported on.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..