cancel
Showing results for 
Search instead for 
Did you mean: 

Using VBUS is not a must

igal
Associate II
Posted on September 03, 2013 at 10:04

I saw an old post that people said VBUS is a must, well, it is not

From the datasheet 30.5 -

''The VBUS pin can be freed by disabling the VBUS sensing option. This is done by setting the

NOVBUSSENS bit in the OTG_FS_GCCFG register. In this case the VBUS is considered

internally to be always at VBUS valid level (5 V).''

It applies to HS as well (different register though)

#vbus
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0