USB host problem
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2014-11-06 12:23 AM
Posted on November 06, 2014 at 09:23
i'm using f407zg and try to use USB HS host with internal PHY but found the program never entry interrupt function
my program is modify form host_device_libV2.10-USB_host_example which i tried on eval board successfullyi already defined USE_EMBEDDED_PHY marco and there are init code: USBH_Init(&USB_OTG_Host, USB_OTG_HS_CORE_ID, &USB_Host, &USBH_MSC_cb, &USR_Callbacks);void USB_OTG_BSP_Init(USB_OTG_CORE_HANDLE *pdev){ GPIO_InitTypeDef GPIO_InitStructure; RCC_AHB1PeriphClockCmd( RCC_AHB1Periph_GPIOB , ENABLE); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_15 | GPIO_Pin_14; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ; GPIO_Init(GPIOB, &GPIO_InitStructure); GPIO_PinAFConfig(GPIOB,GPIO_PinSource15,GPIO_AF_OTG2_FS) ; GPIO_PinAFConfig(GPIOB,GPIO_PinSource14,GPIO_AF_OTG2_FS) ; RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG, ENABLE); RCC_AHB1PeriphClockCmd( RCC_AHB1Periph_OTG_HS, ENABLE) ;}so any advice?
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0