USB and WFI
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2011-12-05 11:46 PM
Posted on December 06, 2011 at 08:46
Hello,
I finally get the USB stack to work on my custom hardware.Last thing I need to fix is that once everything is started I rely only upon interrupts (as the USB stack), so my main method looks like :int main(void){ init(); while(1) __WFI();}But with the USB stack active, it works only if I change the __WFI() intrinsic by __nop().That means the MCU doesn't automatically enters sleep mode between interrupts, and my power consumption increased a lot (by 20/30mA), I cannot really afford that on the LDO.Do anyone have a clue about why the USB stack doesn't work with WFI ?Thomas.[EDIT] Do you think using SLEEPONEXIT would change something ?
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0