cancel
Showing results for 
Search instead for 
Did you mean: 

USART 3 Problem

leventeyigel52
Associate II
Posted on July 18, 2012 at 12:03

Hi ;

I am working on STM32F107VCT6 C-Eval Board and i can work with  usart3 ( smartcard interface)

But when i transport this project to STM32 E-Eval ( STM32F103VGT6) 

byte receive function doesn't work but all the other peripherals are working .

What can we do ? Where's the problem

Can you help me about me ?  
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on July 18, 2012 at 14:10

Hard to say without seeing how you have things coded/wired. The SmartCard is a single pin (RX/TX) interface, right? You should probably review the differences between the Connectivity series parts, and the part you are now using as they have different feature sets.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..