2015-08-24 3:59 AM
Hi all,
I'm using UDP Echo client code example in STM32F217xx.I can send the custom buffer...ok but I can't receive udp packets from PC. I have a VS code that can generate UDP test packets as well... I use the udp_recv function that sets a call back function...I have a breakpoint in callback function...but no packet receive. When I check in wireshark, it says: destination port is unreachable !!! I changed the port but the problem remains... It would be appreciated if you help any way.Thanks2015-08-25 9:32 AM
Hi khoshnoud.borzoo,
Refer to , it can guide you. -Shahrzad-2016-06-14 11:48 AM
Hello khoshnoud.borzoo,
i have the same problem. Did you find the solution?Thanks for your help in advance.Best regards.2016-06-14 11:55 AM
HelloShahrzad,
from the application note its not that obvious what could be the problem with the provided example project. Could you give us some hints, tips? In theudp_client_connect(void) function we define the receive callback byudp_recv(upcb, udp_receive_callback, NULL). I suppose that thevoid udp_receive_callback(void *arg, struct udp_pcb *upcb, struct pbuf *p, const ip_addr_t *addr, u16_t port); shall be called every time a package is received, however i debugged and it is not called. I assume something is missing in the example code..
Thanks for your help in advance.
Best regards.