Trying to use the cube_lib
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-03-05 9:25 AM
Posted on March 05, 2015 at 18:25
Hello all,
Wondering if anyone figured out how to use the sram (stm32f4xx_hal_sram.h) setup to output to various displays .. Having trouble with writing straight to an address port .. With all the ports set up in the gpio under the void HAL_FMC_MspInit(void).. I'm using the StCubeMx program to set things up with ... This is in the alj_port_write.c file: I'm calling the alj_portwrite(); from another c file &sharpinclude <stm32f4xx_hal_conf.h> &sharpinclude ''includes.h'' &sharpdefine adport 0x6C000000 GPIO_InitTypeDef GPIO_InitStructure; int i; void alj_portwrite(void) { // Even though this is in another c file and being called I put this here trying to // make since of what is going on /*Perform the SRAM4 memory initialization sequence*/ SRAM_HandleTypeDef hsram4; FMC_NORSRAM_TimingTypeDef Timing; hsram4.Instance = FMC_NORSRAM_DEVICE; hsram4.Extended = FMC_NORSRAM_EXTENDED_DEVICE; /* hsram4.Init */ hsram4.Init.NSBank = FMC_NORSRAM_BANK4; hsram4.Init.DataAddressMux = FMC_DATA_ADDRESS_MUX_DISABLE; hsram4.Init.MemoryType = FMC_MEMORY_TYPE_SRAM; hsram4.Init.MemoryDataWidth = FMC_NORSRAM_MEM_BUS_WIDTH_16; hsram4.Init.BurstAccessMode = FMC_BURST_ACCESS_MODE_DISABLE; hsram4.Init.WaitSignalPolarity = FMC_WAIT_SIGNAL_POLARITY_LOW; hsram4.Init.WrapMode = FMC_WRAP_MODE_DISABLE; hsram4.Init.WaitSignalActive = FMC_WAIT_TIMING_BEFORE_WS; hsram4.Init.WriteOperation = FMC_WRITE_OPERATION_DISABLE; hsram4.Init.WaitSignal = FMC_WAIT_SIGNAL_DISABLE; hsram4.Init.ExtendedMode = FMC_EXTENDED_MODE_DISABLE; hsram4.Init.AsynchronousWait = FMC_ASYNCHRONOUS_WAIT_ENABLE; hsram4.Init.WriteBurst = FMC_WRITE_BURST_DISABLE; hsram4.Init.ContinuousClock = FMC_CONTINUOUS_CLOCK_SYNC_ONLY; /* Timing */ Timing.AddressSetupTime = 15; Timing.AddressHoldTime = 15; Timing.DataSetupTime = 255; Timing.BusTurnAroundDuration = 15; Timing.CLKDivision = 16; Timing.DataLatency = 17; Timing.AccessMode = FMC_ACCESS_MODE_A; /* ExtTiming */ HAL_SRAM_Init(&hsram4, &Timing, NULL); __GPIOA_CLK_ENABLE(); __GPIOB_CLK_ENABLE(); __GPIOC_CLK_ENABLE(); __GPIOD_CLK_ENABLE(); __GPIOE_CLK_ENABLE(); __GPIOF_CLK_ENABLE(); __GPIOG_CLK_ENABLE(); // end of the mem setup which is in another c file // __FMC_CLK_ENABLE(); // this is in the void HAL_FMC_MspInit(void) also uncommenting this will kill the port ///Diag Leds GPIO_InitStructure.Pin = GPIO_PIN_6; GPIO_InitStructure.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStructure.Speed = GPIO_SPEED_HIGH; HAL_GPIO_Init(GPIOF, &GPIO_InitStructure); GPIO_InitStructure.Pin = GPIO_PIN_1; HAL_GPIO_Init(GPIOC, &GPIO_InitStructure); // SRAM_HandleTypeDef hsram; // hsram.Instance = FMC_NORSRAM_DEVICE; // hsram.Extended = FMC_NORSRAM_EXTENDED_DEVICE; // no setup for which bank in the SRAM_HandleTypeDef function // HAL_SRAM_StateTypeDef ret; &sharpdefine ARRAY_SIZE 2 uint16_t buf1[ARRAY_SIZE]; buf1[1] = 0X55; // Bytes can be sent while the leds are being toggle buf1[2] = 0xAA; // As I found out you can't send 16 bit stuff for(;;) { for ( i = 0 ; i < 20000 ; i++ ) { } *(WORD *)adport = buf1[1]; for ( i = 0 ; i < 20000 ; i++ ) { } *(WORD *)adport = buf1[2]; // have tried using //ret= HAL_SRAM_Write_16b(&hsram, adport, buf1 , ARRAY_SIZE); // but have no understanding of the setup yet as it complains about a casting error for ( i = 0 ; i < 20000 ; i++ ) { } // As I found out commenting these out will result with the address port not working HAL_GPIO_TogglePin(GPIOF, GPIO_PIN_6); HAL_GPIO_TogglePin(GPIOC, GPIO_PIN_1); // Something about toggling the IO ports causes the address ports to work for a brief // period } } #stm32f429 #stm32 #cubemx #sdram
Labels:
- Labels:
-
STM32F4 Series
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0