cancel
Showing results for 
Search instead for 
Did you mean: 

Trigger DMA From CCR Timer

jasonshaw
Associate II
Posted on March 09, 2014 at 20:46

Greetings all, I'm new here so I hope I'm doing this right.

STM32F0

I'm trying to trigger a DMA transfer from TIM2 with CCR1

Here's my code for the timer portion

TIM_TimeBaseInitTypeDef timerInitStructure;

timerInitStructure.TIM_Prescaler = 0;

timerInitStructure.TIM_CounterMode = TIM_CounterMode_Up;

timerInitStructure.TIM_Period = 60;

timerInitStructure.TIM_ClockDivision = TIM_CKD_DIV1;

timerInitStructure.TIM_RepetitionCounter = 0;

TIM_TimeBaseInit(TIM2, &timerInitStructure);

TIM_OCInitTypeDef outputChannelInit;

outputChannelInit.TIM_OCMode = TIM_OCMode_Timing;

outputChannelInit.TIM_OutputState = TIM_OutputState_Enable;

outputChannelInit.TIM_OCPolarity = TIM_OCPolarity_High;

outputChannelInit.TIM_Pulse = 41;

TIM_OC1Init(TIM2, &outputChannelInit);

TIM_OC1PreloadConfig(TIM2, TIM_OCPreload_Enable);

TIM2->DIER |= (0x01 << 14) | (0x01 << 9);

TIM_Cmd(TIM2, ENABLE);

So what I was looking for was being about to trigger a DMA transfer when the count register reaches 41 on DMA1_Channel5.

I can verify that a transfer is happening but it looks like it's happening on Update.

Thanks!

-Jason

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
Posted on March 10, 2014 at 22:41

GPIO_InitTypeDef GPIO_InitStructure;
TIM_OCInitTypeDef TIM_OCInitStructure;
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);
// PA1 - TIM2_CH2
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_Init(GPIOA, &GPIO_InitStructure);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource1, GPIO_AF_2); // PA1 - TIM2_CH2
..
/* Output Compare Toggle Mode configuration: Channel2 */
TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_Toggle;
TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
TIM_OCInitStructure.TIM_Pulse = 14; // Same as CH1 triggering DMA to GPIOB PB[0..2]
TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_Low;
TIM_OC2Init(TIM2, &TIM_OCInitStructure);
TIM_OC2PreloadConfig(TIM2, TIM_OCPreload_Disable);
// Observe phase relationship between TIM2_CH2 EDGEs on PA1 with respect to data latched to GPIOB PB[0..2]. Should be the latency of the DMA servicing
// Suggest DMA table contains 0,1,2,3,4,5,6,7 sequence looped (circular)

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..