cancel
Showing results for 
Search instead for 
Did you mean: 

timer6 strange behaviour

manes6969
Associate II
Posted on August 20, 2011 at 10:21

Hi

I wrote a delay routine using timer6. R2 folds the number of milliseconds to delay.

It works fine , however only from the second time on. the first time there is no delay , the program just 'flies' through the code without a delay.

This is my routine (in assembler)

delayms        ;delay r2 milliseconds

                stmfd    r13!,{r0,r1,r14}        

        

                ldr    r0,=TIM6_CNT        ;start counting from 0000

        mov    r1,#0x0000

        str    r1,[r0]

        ldr    r0,=TIM6_PSC        ;prescaler = 59904 ; gives 1ms/count

        ldr     r1,=59904

        str    r1,[r0]

        ldr    r0,=TIM6_ARR        ;r2 = # milliseconds

        str    r2,[r0]

        ldr    r0,=TIM6_CR1        ;enable counter,no reload, single puls mode

        mov    r1,#0x000d

        str    r1,[r0]

                

delayl        ldr    r0,=TIM6_SR        ;wait for UIF

        ldr    r1,[r0]

        cmp     r1,#0x0000

        beq    delayl        

        ldr    r0,=TIM6_SR        ;clear UIF flag

        mov    r1,#0x0000

        str    r1,[r0]

        ldr    r0,=TIM6_CR1        ;stop the timer

        mov    r1,#0x0000

        str    r1,[r0]

                ldmfd    r13!,{r0,r1,pc}

Does anyone know what the reason could be for this behaviour ?

Any help is welcome !

Ronny Suy

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on August 20, 2011 at 16:36

Without putting it on the bench, I'd be concerned with the status register test and making it more specific, then perhaps look at the loading/reloading of registers.

What frequency are you running the timer at?

It I were just spinning in a loop like this, I'd probably just look at using a free running timer, or cycle counter, and waiting for a timeout delta to expire. The core has a 32-bit cycle counter that should permit times of about a minute to be handled, down to tens of nanoseconds.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..