cancel
Showing results for 
Search instead for 
Did you mean: 

TiM3 problem

aamirali641989
Associate II
Posted on June 14, 2013 at 14:52

I have used APB1 = 30Mhz with 60Mhz to timer. I made following coed for TIM3. I have initialized the TIM3 interrupt.

void TIM3_IRQHandler(void)

{

    TIM3->SR     = 0x0000;              /* clear update flag */

    GPIOA->ODR ^= GPIO_Pin_7;

}

void config_TIM3()

{

    TIM3->CR1     = 0x0084;              /* No clock divder , ARR is buffered , update Event enabled */

    TIM3->SR      = 0x0000;              /* clear interrupt flag */

    TIM3->EGR     = 0x0000;              /* clear interrupt generation bit */

    TIM3->DIER    = 0x0001;              /* enable interrupt flag */

    TIM3->PSC     = 0x0000;              /* no prescaler */ 

    TIM3->CNT     = 0x00000000;          /*  */

    TIM3->ARR     = 0xffff;

    TIM3->CR1    |= 0x0001;              /* enable counter */  

}

Problem is there is timing mismatch

I think I had not configured timer properly.

I am using formula delay_time = ( ARR * (PSC+1) )/PCLK

                                             = (65535 * 1 ) / 60000000 = 1.09225 ms

I am getting 1.164ms. 

For system_init() I have used ST clock config utility(excel sheet).

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0