cancel
Showing results for 
Search instead for 
Did you mean: 

The USB OTG Test results of F4 Discovery

seawwh2
Associate II
Posted on May 13, 2012 at 15:35

1. I can make two VCP at USB HS port and FS port at the same time by Library v2.1.0.

2. Read/Write USB Disk is ok by STM32F4DISCOVERY firmware which is base on OTG Library v2.0.0, It can access any UDisk;

3. Read/Write USB Disk is not good by example of Library v2.1.0. It can only access some UDisk.  For some disk , It can enumerate but stoped at GET_MAX_LUN stage.

Are there any bugs in  Library v2.1.0.?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0