cancel
Showing results for 
Search instead for 
Did you mean: 

Sub-Dollar STM32F3 Floating-Point DSC available in Distributors Stock

Amel NASRI
ST Employee
Posted on April 24, 2014 at 10:55

STM32F30x-Low memory size

 

STM32F301: the cheapest C-M4 in full production!

0690X0000060MmOQAU.gif

N

ew

http://www.st.com/stm32f3-pr

microcontrollers based on the ARM® Cortex®-M4 core with Floating-Point Unit (FPU) are in full production and now in stock at distributors:

STM32F3 devices combine the 72MHz ARM Cortex-M4 core featuring DSP instruction set and FPU with high-performance analog peripherals to bring advanced integration to entry-level mixed-signal control applications.

To help engineers try out new ideas and quickly create prototypes, there are:

STM32F3 Series

http://www.st.com/stm32f3-pr

STM32F3

http://www.st.com/web/en/news/n3547

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0