cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L496VE and Keil ARM-MDK 5

Philipp Bolte
Associate II
Posted on December 06, 2017 at 13:15

Hello,

I am trying to program software for the STM32L496VE MCU with the Keil ARM-MDK 5 IDE. But unfortunatly the Device I am using is not included in the latest Device Feature Pack (Keil::STM32L4xx_DFP). A screenshot of the available devices in the DFP is attached. 

As a workaround I have tryed to select the 

STM32L496VG device (the only difference should be the available flash memory of 1M instead of 512k). I changed the flash memory size in the Tatget settings (changed IROM1 size to 0x8000) and in the Debug Settings. But even then it was not possible to program the controller. The communication via SWD is working, it starts to program but at the end a failure is shown (Error: Flash Download failed - 'Cortex-M4'). I am using a Keil ULINK-ME debugger.

Is there any solution to the problem?

Thank you in advance.

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
AvaTar
Lead
Posted on December 06, 2017 at 13:30

Asking Keil ?

They need some time to integrate new parts in their IDE, and depend on the vendor for information.

Posted on December 06, 2017 at 16:40

But why does it report the ULINK is failing? Do you have a suitable flash algorithm selected? Does it not connect? Does the verify fail?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Philipp Bolte
Associate II
Posted on December 07, 2017 at 08:14

I selected the 1 M version of the MCU, because that version was available in the STM32L4 DFP, and reduced the flash memory size in the Flash settings. But only the 'STM32L4xx 1 M Flash' algorithm is available in the list of programming algorithms. 

For testing purpose I also tried to flash a hex file, that was built for the STM32L496VG (The one with 1 M), with a ST-

LINK 

debugger and the ST-LINK Utility. That was working. The flash process was successful and the program is running.

But for development purposes I need to debug the program with Keil.

Posted on December 07, 2017 at 13:34

So can't you just use the ST-LINK pod in Keil?

The die in your part likely has 1MB of FLASH, I'd expect the algorithm to work, seemed to with the ST-LINK. 

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..