Skip to main content
mmensch
Associate III
June 22, 2016
Question

STM32L152 Nucleo and CubeMX

  • June 22, 2016
  • 2 replies
  • 629 views
Posted on June 22, 2016 at 09:11

Hello,

yesterday I created a small program for STM32L152 Nucleo with CubeMX. It was running but MCO set to HSE gave only 4MHz with 75% duty cycle while I measured OSCin with 8MHz. After searching a while I found that there is a special setting for the HSE oscillator modul when using an external clock signal fed into OSCin. I found this setting prepared with defines in the HAL files and changed this line accordingly:

RCC_OscInitStruct.HSEState = RCC_HSE_BYPASS; //RCC_HSE_ON;

Then everything was fine.

Now my question is if there is a way to use this setting in the clock configuration tab in CubeMX. Otherwise I will have to correct it again any time I create new code with CubeMX.

What seems strange to me is that I found no solution to this problem in the internet. Seems no one noticed before, although both are ST products.

Any help is welcome

Martin

    This topic has been closed for replies.

    2 replies

    Walid FTITI_O
    Visitor II
    June 22, 2016
    Posted on June 22, 2016 at 13:38

    Hi Mr_M_from_G,

    I see now what you have missed. The configuration window at the left of Pinout tab contains the main configuration of the MCU peripheral that you can select/switch. For other detailed configuration , you can go to ''Configuration tab -> Peripheral bottom'' and select/ modify parameters there.

    -Hannibal-
    mmensch
    mmenschAuthor
    Associate III
    June 23, 2016
    Posted on June 23, 2016 at 09:01

    Hello all,

    I found myself, it is in the pinout tab under RCC -> High Speed Clock

    Martin