cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L152 Clock Configuration utility AN3909

valeriogiampa
Associate II
Posted on March 24, 2012 at 20:20

Hi,

there is anyone that use the excel file to configure the RCC of the STM32L152?

When I include in my project the file system_stm32l1xx.c generated with the AN3909, I have same problem in the make process. Same define are not specified. For example the FLASH_BASE value are not defined in the file and in the other stm32 library file.

Can someone help me? 

#an3909-stm32l152-clock-config
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0